This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Codec Engine Examples running error

hello

    I'm trying to build the Codec Engine_3_22_01_06  examples as detailed in the "Build/Run Instructions for Codec Engine Examples" document.  The build for examples/codecs and examples/extensions is successful.  when I run the app on DM8147, I get the following error message:

     root@dm814x-evm:/opt/app# ./app_remote.xv5T
[t=0x000029c4] [tid=0x400d9000] ti.sdo.xdcruntime.linux.ThreadSupport: ERROR: line 241: E_POSIX_Error: a POSIX function returned failure, errno is 0
ti.sdo.xdcruntime.linux.ThreadSupport: line 241: E_POSIX_Error: a POSIX function returned failure, errno is 0
xdc.runtime.Error.raise: terminating execution

     when I exported CE_DEBUG=3

    the error msg is

    [t=0x000530ee] [tid=0x40061000] ti.sdo.ce.osal.Global: [+E] Global_atexit> Enter (fxn=0x26a8c)
[t=0x00053174] [tid=0x40061000] ti.sdo.ce.osal.Global: [+E] Global_atexit> Enter (fxn=0x2366c)
[t=0x00053208] [tid=0x40061000] ti.sdo.ce.ipc.Processor: [+2] Processor_init> SysLink_setup()...
[t=0x000558a2] [tid=0x40061000] ti.sdo.ce.ipc.Processor: [+2] Processor_init> ... SysLink_setup() done
[t=0x00055970] [tid=0x40061000] ti.sdo.xdcruntime.linux.ThreadSupport: ERROR: line 241: E_POSIX_Error: a POSIX function returned failure, errno is 0
ti.sdo.xdcruntime.linux.ThreadSupport: line 241: E_POSIX_Error: a POSIX function returned failure, errno is 0
xdc.runtime.Error.raise: terminating execution

     can anyone give me some help? thanks!

  • Hello,

    If you are using EZSDK, you should follow the below doc:

    http://downloads.ti.com/dsps/dsps_public_sw/ezsdk/latest/exports/DM814x_EZ_Software_Developers_Guide.pdf

    section 3.3 Running the Codec Engine examples

    ll55028 said:
    root@dm814x-evm:/opt/app# ./app_remote.xv5T


    You will find that there are several steps before that one.

    Best regards,
    Pavel

  • hello

           I am using rdk_ipnc v3.5.

           i just insert syslink.ko and cmemk.ko then run

           root@dm814x-evm:/opt/app# ./app_remote.xv5T