This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Building sgx modules for linux-omap 2.6.32

I am attempting to build the latest omap3-sgx-modules-1.4.14.2514 for linux-omap 2.6.32.

The build completes without errors.

However when I attempt to load the omaplfb module I get the following error:

omaplfb: OMAPLFB_Init: OMAPLFBInit failed

I spent a bit of time looking into this and it seems that I get an OMAP_ERROR_DEVICE_REGISTER_FAILED error return from OMAPLFBInit in omaplfb_displayclass.c

Has anyone else had success with this latest revision of the code and linux-omap 2.6.32?

Also, what is the proper way to enable the debug messages in the code?

Steve