Hello:
I use dvrdk350,when I use ths8200 to output VGA,when set resolution as 1080P60 or 720P60,there a line on the display left,some time is blue,some time is green.but HDMI display is OK(use DVO2 to display)
when I don't put any data to display,still have a bright line on the right,so i think mabe HDVPSS driver have bug?
my link data flow is: capture -->sclar-->swms-->display(ths8200)
no data send to display:
send a stream to display,on the right still have a green line:
read 720P THS8200 register config:
{0x0,0x0},
{0x1,0x0},
{0x2,0x4},
{0x3,0x1},
{0x4,0x81},
{0x5,0xd5},
{0x6,0x0},
{0x7,0x0},
{0x8,0x6},
{0x9,0x29},
{0xa,0x4},
{0xb,0x0},
{0xc,0x4},
{0xd,0x80},
{0xe,0x4},
{0xf,0x0},
{0x10,0x80},
{0x11,0xbb},
{0x12,0x7},
{0x13,0x42},
{0x14,0x0},
{0x15,0x0},
{0x16,0x14},
{0x17,0xae},
{0x18,0x8b},
{0x19,0x15},
{0x1a,0x0},
{0x1b,0x0},
{0x1c,0x73},
{0x1d,0x0},
{0x1e,0x80},
{0x1f,0x80},
{0x20,0x0},
{0x21,0x0},
{0x22,0x0},
{0x23,0x23},
{0x24,0x2a},
{0x25,0x28},
{0x26,0x6e},
{0x27,0x28},
{0x28,0x4},
{0x29,0x0},
{0x2a,0x4},
{0x2b,0xc0},
{0x2c,0x0},
{0x2d,0x0},
{0x2e,0x0},
{0x2f,0x6e},
{0x30,0x0},
{0x31,0x0},
{0x32,0x0},
{0x33,0x0},
{0x34,0x6},
{0x35,0x72},
{0x36,0x0},
{0x37,0x1},
{0x38,0x87},
{0x39,0x22},
{0x3a,0xee},
{0x3b,0xee},
{0x3c,0x80},
{0x3d,0x0},
{0x3e,0x0},
{0x3f,0x0},
{0x40,0x0},
{0x41,0x40},
{0x42,0x40},
{0x43,0x40},
{0x44,0x53},
{0x45,0x3f},
{0x46,0x3f},
{0x47,0x40},
{0x48,0x40},
{0x49,0x40},
{0x4a,0xfc},
{0x4b,0x44},
{0x4c,0xac},
{0x4d,0xac},
{0x4e,0xac},
{0x4f,0xff},
{0x50,0x0},
{0x51,0x22},
{0x52,0x0},
{0x53,0x0},
{0x54,0x0},
{0x55,0x0},
{0x56,0x0},
{0x57,0x0},
{0x58,0x6},
{0x59,0x1a},
{0x5a,0xea},
{0x5b,0xef},
{0x5c,0x0},
{0x5d,0x0},
{0x5e,0x0},
{0x5f,0x0},
{0x60,0x0},
{0x61,0x0},
{0x62,0x0},
{0x63,0x0},
{0x64,0x0},
{0x65,0x0},
{0x66,0x0},
{0x67,0x0},
{0x68,0x21},
{0x69,0x1},
{0x6a,0x0},
{0x6b,0x0},
{0x6c,0x0},
{0x6d,0x0},
{0x6e,0x0},
{0x6f,0x0},
{0x70,0x70},
{0x71,0x0},
{0x72,0x1},
{0x73,0x4},
{0x74,0x0},
{0x75,0x1},
{0x76,0x0},
{0x77,0x7},
{0x78,0xff},
{0x79,0x0},
{0x7a,0x28},
{0x7b,0x0},
{0x7c,0x5},
{0x7d,0x6},
{0x7e,0x72},
{0x7f,0x72},
{0x80,0xee},
{0x81,0x0},
{0x82,0x63},
{0x83,0x0},
{0x84,0x0},
{0x85,0x0},
if anyone have met this probrem,please told me,thanks very much!