This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

using tvp5158 and dm6437 clock problem

Other Parts Discussed in Thread: TVP5158

I just want there is only one clock source(27Mhz cystal), and I don't need audio input , just need 4-ch half D1 vedio input from tvp5158 using line-interleveaed mode to DM6437, Is that possible?

I want to know if I can connect the  tvp5158's XTAL_IN pin  to the Dm6437's CLKOUT0 pin,

make the output clock of DM6437 as the tvp5158's clock source,

Is that pollsible?

thank you