This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can I use Match mode for triggering accurate DMTimer 1ms interrupts instead of Overflow?



Hello, 

I have a working 1ms timer using the DMTimer 1ms and overflow mode with autoreload, but have a question.  Is there some reason that the documentation for setting up the 1ms timer on the AM335x processor only describes using Overflow Mode for accurate 1ms intervals?  Typically timers are set up to trigger an interrupt on a Match event, instead of Overflow.  Is there a method of using Match, or is there some solid reason that the documentation examples only use Overflow Mode for achieving that?

Thank you,