This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART4 registration to linux kernel

Hello,

How to disable registering UART4 of omap4460 processor to Linux kernel-3.4?

I had configured CONFIG_SERIAL_8250_NR_UARTS and CONFIG_SERIAL_8250_RUNTIME_UARTS to 3 still UART4 gets registered during linux boot.

Regards,

Parimala

  • Hello Parimala,

    You configure the cernel to register 3 UART devices, right?  I think that the problem is as follows:
    According to OMAP4460 TRM, Section 23.3.1 UART/IrDA/CIR Overview, the device contains four UART devices controlled by the MPU:
    • Three UART-only modules (UART1, UART2, and UART4) are pinned out for use as UART devices
    only.
    • UART3, which adds infrared communication support, is pinned out for use as a UART, IrDA, or CIR
    device, and can be programmed to any available operating mode.

    Typically UART3 is used as IrDA interface, so when configureing CONFIG_SERIAL_8250_NR_UARTS & CONFIG_SERIAL_8250_RUNTIME_UARTS to 3 you register UART1, UART2 and UART4 devices.

    Best Regards,
    Yordan

  • Hello Yordan,

    Thank you for the reply.

    If I give CONFIG_SERIAL_8250_RUNTIME_UARTS & CONFIG_SERIAL_8250_NR_UARTS to 2 also all the 4 uarts gets registered during kernel boot. following is the boot log

    [    0.729522] Serial: 8250/16550 driver, 2 ports, IRQ sharing enabled
    [    0.730773] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 104) is a OMAP UART0
    [    0.731231] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 105) is a OMAP UART1
    [    0.731719] omap_uart.2: ttyO2 at MMIO 0x48020000 (irq = 106) is a OMAP UART2
    [    1.779205] console [ttyO2] enabled
    [    1.783386] omap_uart.3: ttyO3 at MMIO 0x4806e000 (irq = 102) is a OMAP UART3

    and "cat /proc/iomem" too shows memory allocations for all the UARTS.

    Why the kernel configurations are ineffective in this case?

    Regards,

    Parimala

  • Hello Parimala,

    You are making these modifications to kernel/arch/arm/configs/android_omap_defconfig, right?

    Also, which OS are you using (my guess is Android)?

    Best Regards,

    Yordan

  • Hello Yordan,

    I am using Linux OS, not the Android.

    I have a pandaboard es hardware and I am doing the following steps to compile linux kernel

    make omap4plus_defconfig

    make menuconfig(to configure number of UARTS)

    make uImage

    Thank  you.

    Regards,

    parimala