Hi all,
I want to control a multiplexer using my TMS320C6748 DSP and the CCSv5, is it possible? How can I do it? Can I control the voltage from the logic outputs?
These are the two mux that I want to control:
http://pdf.datasheetcatalog.com/datasheets/185/420758_DS.pdf
http://www.analog.com/static/imported-files/data_sheets/ADG1604.pdf
The main idea is to use both mux to switch between different input and output audio signals.
Thanks in advance,
Miguel.