This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can not USE L1P and L1D memory sections together.

Hi,

I have one function say, FUNC and a buffer say BUFF.

when i am allocating FUNC in L1P memory and BUFF in L1D memory. DSP(C674x) is going in reset. (, after loading the .OUT file,cursor is not coming at starting point( void main() ) and it start running itself, and then goes into reset)

if i am using L1P memory  for FUNC  n BUFF ,then thing are working.leaving L1D untouched.

also,when i am using L1D memory  for FUNC  n BUFF ,then thing are working.leaving L1P untouched.

i don't know , why i am not able to use L1P n L1D memory sections simultaneously.

Thanks.