This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

To prevent the bridge transmission in Dual MAC Mode

Guru 10105 points
Other Parts Discussed in Thread: AM3352

Hi all,
When operating in Dual Mac Mode with AM335x
it is set as vlan_member_list = 0x1 of ALE VLAN Table Entry
to prevent transferring packets between port1 and port2.
This setting is that the port0 is only associated VLAN.
Is my understanding correct?

[Status]
-OS: SDKv7 Linux Kernel-3.12.x
-EVM: Custom with AM3352

Best regards,
Kanae

  • Hi Kanae,

    This post has an excellent description of the CPSW behavior in different modes: http://e2e.ti.com/support/arm/sitara_arm/f/791/p/336582/1174988.aspx#1174988

  • Hi Biser,

    Thank you for your quick reply.
    I have checked the post you mentioned.
    So I would like to make sure that the external ports; port1 and port2
    do not transfer packets each other when I configure the dual MAC mode
    and set as vlan_member_list = 0x1 of ALE VLAN Table Entry.
    If not configuring dual MAC mode, the external ports; port1 and port2 transfer
    packets each other.

    Could you please point if my understanding is wrong?

    Best regards,
    Kanae

  • See section 14.3.2.10.2 in the AM335x TRM Rev. J. What you require is described there.

  • Hi Biser,

    Thank you for your suggestion.
    I think my explanation was not enough in my past post.

    When only port 0 is set as vlan_member_list = 0x1 of ALE VLAN Table Entry
    and port 1 and port 2 are not set as vlan member list, the packet transfers operate
    actually as follows.

    [Vlan tagged packet]

     port0 <-> port1 :vlan packets can transfer.

     port0 <-> port2: vlan packets can transfer.

     port1 <-> port2: vlan packets cannot transfer.


    It seems from this result that the transfer operation from port0 to port1/port2
    is effective regardless of vlan member list setting.

    I suppose this is inconsistent with what TRM described in 14.3.2.10.2 Dual Mac Mode.
    =========
    Configure the Port 1 to Port 0 VLAN

    Add a VLAN Table Entry with ports 0 and 1 as members (clear the flood masks).

    ...
    Configure the Port 2 to Port 0 VLAN

    Add a VLAN Table Entry with ports 0 and 2 as members (clear the flood masks).
    ===========

    When adding a VLAN Table with ports 0 and 1 as members or ports 0 and 2 as members,
    the packet transfers start from port 2 to port 1.
    This result is also inconsistent with what TRM described in 14.3.2.10.2 Dual Mac Mode.

    That is why I would like to make sure the proper way to prevent transferring packets
    between port1 and port2.  


    Best regards,
    Kanae

  • Kanae,

    Enabling Dual MAC mode will prevent downstream port peering (direct xfer between ports 1&2) by default. I believe this is what you are looking to do.

  • Hi DK,

    Thank you for your reply.
    I understand there is totally no problem to AM335x H/W function by your reply.
    Our issue to downstream port peering (direct xfer between ports 1&2) must be caused by TI SDK Linux driver.
    The release notes describe “D-01525: In Dual EMAC mode the device will fail to receive a DHCP address from some routers. Use single EMAC mode. This is under investigation.” as a known issue.

    I would like to ask you whether only port 0 is set as vlan_member_list = 0x1 of ALE VLAN Table Entry would be a workaround for this issue, or not?

    Any comments would be appreciated.

    Best regards,
    Kanae