Hi,
When I'm loading a program to a 6654 for a debug session I obtain this.
This occured on 6 boards in a batch of 29 boards.
CCS version : Version: 5.4.0.00091
Emulator : Blackhawk USB560 v2 system trace.
Any Idea ?
Thanks to all
Console printout :
[C66xx_0] 0 A1=0xffff0001
A2=0x0 A3=0x4000
A4=0xe A5=0x0
A6=0x0 A7=0x0
A8=0x1 A9=0x0
A10=0x814dd0 A11=0x804bd8
A12=0x814dd0 A13=0x2200000
A14=0x814b70 A15=0x813888
A16=0x42 A17=0x42000000
A18=0x7f000000 A19=0x7f0000
A20=0x0 A21=0x0
A22=0x8b31c4 A23=0x8b2f30
A24=0x0 A25=0x40450000
A26=0x5 A27=0x8b2fd8
A28=0x400 A29=0x1
A30=0x1 A31=0x180010c
B0=0x0 B1=0x0
B2=0x0 B3=0x809318
B4=0x2200000 B5=0x0
B6=0x0 B7=0x814dd0
B8=0x90 B9=0x1
B10=0x15000100 B11=0x803e74
B12=0x0 B13=0x80d8ac
B14=0x0 B15=0x814890
B16=0x814e60 B17=0x8cac94
B18=0x894281 B19=0x8b2e10
B20=0x0 B21=0x69
B22=0xffffffff B23=0xfffffffa
B24=0x8b3058 B25=0xbfc1f8f7
B26=0xd02c B27=0x0
B28=0x0 B29=0x1
B30=0x8cbf74 B31=0x400000
NTSR=0x10000
ITSR=0x0
IRP=0x0
SSR=0x0
AMR=0x0
RILC=0x0
ILC=0x0
Exception at 0x80d440
EFR=0x0 NRP=0x80d440
ti.sysbios.family.c64p.Exception: line 255: E_exceptionMin: pc = 0x0080d440, sp = 0x00814890.
To see more exception detail, use ROV or set 'ti.sysbios.family.c64p.Exception.enablePrint = true;'
xdc.runtime.Error.raise: terminating execution