This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Auto detect RAM size



Hi,

i don't have much experience to software embedded. I work with am335x pocessor in Linux ubuntu. My board have a 256 MiB RAM. I use the file source code u-boot-2011.09. I have to realize the function that read automatically the size of DDR3 RAM.

In file board.c i have add this row code:

static int display_dram_config(void)
{
    int i;
    unsigned long *p_write_ram = NULL;

#ifndef DEBUG
    puts("RAM Configuration:\n");

    for (i = 0; i < CONFIG_NR_DRAM_BANKS; i++)
      {
        printf("Bank #%d: %08lx ", i, gd->bd->bi_dram[i].start);
        print_size(gd->bd->bi_dram[i].size, "\n");
      }
#else
    ulong size = 0;

    for (i = 0; i < CONFIG_NR_DRAM_BANKS; i++)
            {
        size += gd->bd->bi_dram[i].size;
            }        

    puts("DRAM:  ");
      
        /*TODO: row add to original code*/    
         
         p_write_ram  = 0x80000000;                                         // first address ddr RAM 256MiB
        *p_write_ram = 0xABCDEF00;
         printf("%x %x \n", p_write_ram, *p_write_ram);


         p_write_ram = 0x90000000;
         printf("%x %x \n", p_write_ram, *p_write_ram);

#endif


    return (0);
}

0x80000000 is the first address to write in RAM block 0

0x90000000 is the second address to write in RAM block 1

Either the size block is 256MiB.

In the file am335_evm.h i modify the following #define

#define CONFIG_NR_DRAM_BANKS        2                         /* 2 bank of DRAM */
#define PHYS_DRAM_1                                0x80000000    /* DRAM Bank #1 */
#define PHYS_DRAM_2                                0x90000000    /* DRAM Bank #2 */

#define PHYS_DRAM_1_SIZE                     0x10000000    /* 256 MiB */

#define CONFIG_SYS_SDRAM_BASE        PHYS_DRAM_1
#define CONFIG_SYS_SDRAM_BASE_2    PHYS_DRAM_2

In the code i write to address 0x80000000 the value 0xABCDEF00. After i read the value from address 0x90000000 and i read the same value of the address 0x80000000. Why the two address have the same value?

How can i realize the function that automatically read the size of RAM of my board? For example if my board mount RAM 512, the function return me 512.

Thanks