I'm working on vayu board (Vision High 28) / CortexA15 using GNU compiler.
Since I have to build my own RTCS platform I used the platform wizard. For the original platform everything works, the modified platform produces the following linker error.
c:/ti/ccsv5/tools/compiler/gcc-arm-none-eabi-4_7-2012q4/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/bin/ld.exe:./configPkg/linker.cmd:14: warning: memory region `EXT_RAM' not declared
c:/ti/ccsv5/tools/compiler/gcc-arm-none-eabi-4_7-2012q4/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/bin/ld.exe: .gnu.attributes not found for insert
The problem can simply reproduced executing the following steps.
- Create GNU project: SYS/BIOS->GNU Target Examples->Typical
- File -> New -> Other... -> Edit/View RTSC Platform
- Package Name = ti.platforms.evmDRA7XX
- CPU Core GPP
- Press "Next"
- Select "EXT_RAM" for all memory sections
- Press "Finish"
The "new" platform (nothing was changed compared to the original one) produces the error above when linking.
Here's a list of the relevant tool versions I'm using:
- Code Composer Studio Version 5.5.0.00077
- GCC ARM Compiler Tools 4.7.2012.12
- XDCTools 3.25.3.72
Thanks in advance for any helping answer (I'm currently blocked because of theat issue).
Kind regards,
Roland