Dear all,
i am working on AM335x GP EVM having few quiries in starter ware USB library.
Our requirement is connect a Communication Device like Wi-fi to one of the USB ports and pass the data through another USB port(just bypass the data from initialization,no data Processing at all).
1.Is Starterware USB library(version 2.00.00.07) supports CDC in HOST mode?
2.If it doesn't support what would be the better approach should i follow?
3.is there any USB sacks that supports the HOST for CDC mode compatible to AM335x SOC?
Thanks & Regards
Rama Krishna