Other Parts Discussed in Thread: TVP5147
I have a CCD camera with params is:
pixel: PAL:512H×582V NTSC:512H×492V
output : 1.0Vp-p/75Ω BNC CVBS
but the EVM-DM6467T using TVP5147:with following format
I don't know what the relationship between the CCD camera's pixel 512H×582V and TVP5147's pixel 720x625 ?
Can TVP5147 decode the CCD's CVBS video singal input?
How to program TVP5147 or DM6467T's VPIF register to capture a frame image from CCD camera with PAL fomat ?