Can you please let me know, in MUXED mode, for NOR boot, as such the ROM code will have access to how many Address lines and How much of size of NOR flash?
As per the TRM it says AD0 to AD15, does that mean 64Kilo Bytes?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you please let me know, in MUXED mode, for NOR boot, as such the ROM code will have access to how many Address lines and How much of size of NOR flash?
As per the TRM it says AD0 to AD15, does that mean 64Kilo Bytes?
Check section 26.1.7.2.2 in the TRM. A12 to A27 are not initialized by the ROM code.
In that section, it is mentioned that from A16 above for the Muxed mode. Is that correct? The ROM code can access upto A15 address lines in muxed mode. Right???
From TRM 26.1.7.2.2 Pins Used
"Similarly for Muxed NOR Boot, address lines A16 and above to the memory
are not controlled by the ROM and need to be managed externally during boot to ensure proper
addressing to the all memory signals"