This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Build AM335x StarterWare using GCC

Genius 5785 points


Hello,

I'd like to build AM335x StarterWare in CCSv5.5 using GCC. I referred to below. It looks like easy, but I can't. Is there anyone who can build it?
http://processors.wiki.ti.com/index.php/Building_Starterware_projects_in_CCSv5_using_GCC

Step1: same.

Step2: almost same. My StarterWare version is 02_00_01_01. I uncheck "Show only available toolchain that support this platform" and choose Cygwin gcc. But actually I didn't install Cygwin.

Step3: same.

Step4: I installed CodeSourcery Toolchain as IA32 Windows installer. LIB_PATH is "C:/Program Files (x86)/CodeSourcery/Sourcery G++ Lite". This is default install path.
http://processors.wiki.ti.com/index.php/Installing_CodeSourcery_Toolchain

Step5: There is a error below even though I build project.

Info: Configuration "Default" uses tool-chain "cdt.managedbuild.toolchain.gnu.cygwin.base" that is unsupported on this system, attempting to build anyway.
make all
Cannot run program "make": Launching failed

Error: Program "make" not found in PATH
PATH=[C:/ti/ccsv5/eclipse/jre/bin/client;C:/ti/ccsv5/eclipse/jre/bin;C:/ti/ccsv5/eclipse/jre/lib/i386;C:\Program Files (x86)\CodeSourcery\Sourcery G++ Lite\bin;C:/ti/xdctools_3_23_04_60;C:\Program Files (x86)\Intel\iCLS Client\;C:\Program Files\Intel\iCLS
......

Could you tell me advice?

Regards,
Kazu