This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Conflicting tool versions for networking applications

NSP client example doesn't work with the following tool set:

SYS/BIOS  6.37.02.27
XDCTOOLS  3.25.05.94
NDK       2.22.03.20
NSP VAYU  4.08.00.01

When running the client example on CENTAURUS (Vision Mid EVE) CortexA8 I'm got no ping response from evm.
Just downgrading to older SYS/BIOS 6.35.04.50 resolves that issue.

Besides the "client" demo my CENTAURUS application uses the older "nsp_dm814x_01_00_00_10" instead of Vayu-NSP. In combination with the BIOS/XDC/NDK versions above I can receive all network packets but cannot send "bigger" ones (>2KiB).

Trying various combinations (I cannot name them all) results only in compiler errors due to incompatible API changes, so I didn't succeed.

Is there a tool combination that is verified for both CENTAURUS (Vision Mid EVE) and VAYU (Vision High 28)?
Please be aware the SYS/BIOS version is hard to change due to software organization structure inside the whole company.

Thank you in advance
Roland