Good morning everbody,
At the moment I am testing out Starterware on the Beaglebone. I'm wondering how much better the performance is compared to a Mikrocontroller like the Arduino Due with its 84 MHz or the STM32F4 Discoveryboard with a Cortex-M4 (168MHz). I know that this is a question that has man aspects like whether the Conrtoller uses a FPU etc.
The Sitara Processor with its Cortex-A8 on the Beaglebone is clocked with 700MHz and has a FPU, so I guess it should speed out the Mikrocontrollerboars enormous.
Did anyone made some direct comparison so far?