I have two same board, one of boards have problem when running same software. Sometimes when I enable my enhance alg, the program run fault. I have no idea where is the strange problem. Look forward to your reply, thank you.
The fault is following,
situation 1:
[m3vpss ] Unhandled Exception: [m3vpss ] Exception occurred in ThreadType_Task [m3vpss ] handle: 0x3c9b57b0. [m3vpss ] stack base: 0x3c8e4380. [m3vpss ] stack size: 0x8000. [m3vpss ] R0 = 0x0000b0b0 R8 = 0x3bfe2030 [m3vpss ] R1 = 0x00000000 R9 = 0x0005e3fc [m3vpss ] R2 = 0x3c03fd74 R10 = 0x0005dd80 [m3vpss ] R3 = 0x00001254 R11 = 0x00000000 [m3vpss ] R4 = 0x3c03fd74 R12 = 0x9b70c771 [m3vpss ] R5 = 0x00000000 SP(R13) = 0x3c8ec288 [m3vpss ] R6 = 0x00000021 LR(R14) = 0x9b70c7df [m3vpss ] R7 = 0x00001264 PC(R15) = 0x00437244 [m3vpss ] PSR = 0x21000000 [m3vpss ] ICSR = 0x00400803 [m3vpss ] MMFSR = 0x00 [m3vpss ] BFSR = 0x82 [m3vpss ] UFSR = 0x0000 [m3vpss ] HFSR = 0x40000000 [m3vpss ] DFSR = 0x00000000 [m3vpss ] MMAR = 0x0000c304 [m3vpss ] BFAR = 0x0000c304 [m3vpss ] AFSR = 0x00000000 [m3vpss ] Terminating Execution...
situation2:
[c6xdsp ] ***** VIDEO Firmware build time 15:17:40 Apr 16 2014 EDG gcc 3.0 mode [c6xdsp ] ***** SYSTEM : Frequency <ORG> - 1000000000, <NEW> - 1000000000
situation 3:
[m3vpss ] Unhandled Exception:
[m3vpss ] Exception occurred in ThreadType_Task
[m3vpss ] handle: 0x3c9b57b0.
[m3vpss ] stack base: 0x3c8e4380.
[m3vpss ] stack size: 0x8000.
[m3vpss ] R0 = 0x0000b0b0 R8 = 0x3bfe2030
[m3vpss ] R1 = 0x00000000 R9 = 0x0005e3fc
[m3vpss ] R2 = 0x3c03fd74 R10 = 0x0005dd80
[m3vpss ] R3 = 0x00001254 R11 = 0x00000000
[m3vpss ] R4 = 0x3c03fd74 R12 = 0x9b70c771
[m3vpss ] R5 = 0x00000000 SP(R13) = 0x3c8ec288
[m3vpss ] R6 = 0x00000021 LR(R14) = 0x9b70c7df
[m3vpss ] R7 = 0x00001264 PC(R15) = 0x00437244
[m3vpss ] PSR = 0x21000000
[m3vpss ] ICSR = 0x00400803
[m3vpss ] MMFSR = 0x00
[m3vpss ] BFSR = 0x82
[m3vpss ] UFSR = 0x0000
[m3vpss ] HFSR = 0x40000000
[m3vpss ] DFSR = 0x00000000
[m3vpss ] MMAR = 0x0000c304
[m3vpss ] BFAR = 0x0000c304
[m3vpss ] AFSR = 0x00000000
[m3vpss ] Terminating Execution...
situation 4:
[m3video] Unhandled Exception: [m3video] Exception occurred in ThreadType_SWI [m3video] handle: 0x9a8a0f68. [m3video] stack base: 0x3b59ed84. [m3video] stack size: 0x4000. [m3video] R0 = 0x00000024 R8 = 0x00000001 [m3video] R1 = 0x00000000 R9 = 0x000fd7ea [m3video] R2 = 0x9a860835 R10 = 0x9a82cc9c [m3video] R3 = 0x00000001 R11 = 0x9a82cf48 [m3video] R4 = 0x6365db74 R12 = 0x9a8616dc [m3video] R5 = 0x6365db74 SP(R13) = 0x3b5a2c80 [m3video] R6 = 0x9a8a0d60 LR(R14) = 0x9a85da5b [m3video] R7 = 0x9a82cc88 PC(R15) = 0x9a8608b8 [m3video] PSR = 0x31000000 [m3video] ICSR = 0x00400803 [m3video] MMFSR = 0x00 [m3video] BFSR = 0x82 [m3video] UFSR = 0x0000 [m3video] HFSR = 0x40000000 [m3video] DFSR = 0x00000000 [m3video] MMAR = 0x6365db74 [m3video] BFAR = 0x6365db74 [m3video] AFSR = 0x00000000 [m3video] Terminating Execution...
situation 5:
[m3video] Unhandled Exception: [m3video] Exception occurred in ThreadType_Task [m3video] handle: 0x3b2f1c94. [m3video] stack base: 0x3b590000. [m3video] stack size: 0x2000. [m3video] R0 = 0x00071d3a R8 = 0x59000000 [m3video] R1 = 0x00000000 R9 = 0x590276c6 [m3video] R2 = 0x00000000 R10 = 0x3ab31e80 [m3video] R3 = 0x00000000 R11 = 0x3ab2f38a [m3video] R4 = 0x0000195c R12 = 0x00000002 [m3video] R5 = 0x3ab31e80 SP(R13) = 0x3b591a68 [m3video] R6 = 0x59027540 LR(R14) = 0x00000000 [m3video] R7 = 0x000010c4 PC(R15) = 0x9a8686c0 [m3video] PSR = 0x61000000 [m3video] ICSR = 0x0440f803 [m3video] MMFSR = 0x00 [m3video] BFSR = 0x82 [m3video] UFSR = 0x0001 [m3video] HFSR = 0x40000000 [m3video] DFSR = 0x00000000 [m3video] MMAR = 0xffffcf20 [m3video] BFAR = 0xffffcf20 [m3video] AFSR = 0x00000000 [m3video] Terminating Execution...
situation 6:
[m3video] !!!XDC RUNTIME ASSERT FAILED [m3video] xdc.runtime.Error @ line 86: [m3video] assertion failure: A_initializedParams: uninitialized Params struct
situation 7:
sometimes have no any print information, but video stopped.