Hi,
I set the bootmode pins [0-12] as 0100 0010 0111 0 when I was trying ethernet boot. But it failed. I captured some BOOTP packets using wireshark. The source IP of the BOOTP packet is 0.0.0., then I tried the command line: arp -s 192.168.1.2 40-5f-c2-c0-da-5e,the mac address derived from the BOOTP packed. Unfortunately, there is nothing changed, the C6678 keep on seeding BOOTP packets and it's source ip is still 0.0.0.0. I can't send .eth file to that c6678.
Are there any other things I need to do?
Additionally, I want to know is there something to do with IBL which stored in EEPROM when Ethernet boot mode is applied.
Regards,
Philly.