hi to all..
I am trying to build for DM368, IPNC.
It's no problem to build by uboot-lspcfg-dvsdk.
It's occurred to make lspbuild.
My environment is Window 7_64, Vmware Ubuntu 12.04_32bit.
I have a face to a problem is as below...
LD kernel/built-in.o
LD drivers/char/built-in.o
drivers/char/irqk.o: In function `init_module':
irqk.c:(.init.text+0x0): multiple definition of `init_module'
drivers/char/edmak.o:edmak.c:(.init.text+0x0): first defined here
drivers/char/irqk.o: In function `cleanup_module':
irqk.c:(.exit.text+0x0): multiple definition of `cleanup_module'
drivers/char/edmak.o:edmak.c:(.exit.text+0x0): first defined here
drivers/char/dm365mmap.o: In function `init_module':
dm365mmap.c:(.init.text+0x0): multiple definition of `init_module'
drivers/char/edmak.o:edmak.c:(.init.text+0x0): first defined here
drivers/char/dm365mmap.o: In function `cleanup_module':
dm365mmap.c:(.exit.text+0x0): multiple definition of `cleanup_module'
drivers/char/edmak.o:edmak.c:(.exit.text+0x0): first defined here
drivers/char/cmemk.o: In function `init_module':
cmemk.c:(.init.text+0x0): multiple definition of `init_module'
drivers/char/edmak.o:edmak.c:(.init.text+0x0): first defined here
drivers/char/cmemk.o: In function `cleanup_module':
cmemk.c:(.exit.text+0x0): multiple definition of `cleanup_module'
drivers/char/edmak.o:edmak.c:(.exit.text+0x0): first defined here
make[4]: *** [drivers/char/built-in.o] Error 1
make[3]: *** [drivers/char] Error 2
File structure is as below..
.
├── dvsdk_2_10_01_18
│ ├── bin
│ ├── cg_xml_2_12_00
│ ├── clips
│ ├── codec_engine_2_24
│ ├── dm365_codecs_01_00_06
│ ├── dm365mm
│ ├── dmai_1_21_00_10
│ ├── docs
│ ├── dvsdk_demos_2_10_00_17
│ ├── dvtb_4_10_03
│ ├── edma3_lld_1_06_00_01
│ ├── examples
│ ├── framework_components_2_25_00_04
│ ├── kernel_binaries
│ ├── licenses
│ ├── linuxutils_2_24_03
│ ├── PSP_02_10_00_14
│ ├── quilt
│ ├── xdais_6_24
│ └── xdctools_3_15_01_59
└── ipnc
├── av_capture
├── ipnc_app
├── ipnc_psp
├── ipnc_rdk
├── tftp
└── ti-davinci
I have solved various building issues but I don't know why it was occurred..
How can I do..?
So, anybody please help me..
Thanks a lot in advice.