This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

svg library (librsvg) not present in sdk-am335x-evm-06.00.00.00

Hi,

Iam using AM335x starter kit (TMDSSK3358 EVM). I was developing an application for svg overlay in gstreamer(using rsvgoverlay element) in "ti-sdk-am335x-evm-05.05.00.00" SDK. The application works fine in this sdk.  As i had to implement the adc feature to this application, i switched to  "ti-sdk-am335x-evm-06.00.00.00". But the latter sdk does have many packages that was present in the former for example librsvg, pango, gtk+ etc... Kindly let me know what was the reason for removing these packages from the sdk-6. 

So iam not able to implement the application in sdk6.

I need librsvg for overlaying svg that was not present in the latter sdk. So i tried cross compiling the package. I was not able to cross compile the package due to its dependencies that was not present in software manifest of latter sdk.

Is there any feeds that contain all the packages so that i can install the required packages for the sdk6. 

Else can i get a prebuild rootfs with the librsvg library installed in it... 

please do help me at the earliest...

Any help would be much appreciated.

Waiting for your reply...