This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

No debug print after Linux kernel starting OMAPL138

Other Parts Discussed in Thread: OMAPL138, DA8XX

Hello,

I do not get output after line Starting kernel ...

I have found the relevant Troubleshooting page in the TI Wiki, a couple of posts here but so far failed to get the prints. 

My u-boot configuration

bootargs console=ttyS0,115200n8 root=/dev/nfs noinitrd nfsroot=10.0.0.45:/var/www/share/fs,nolock,rsize=1024,wsize=1024 ip=10.0.0.148

In the hardware low level initialization code (head.S) I did following

setmode PSR_F_BIT | PSR_I_BIT | SVC_MODE, r9 @ ensure svc mode
@ and irqs disabled

mrc p15, 0, r9, c0, c0 @ get processor id
bl __lookup_processor_type @ r5=procinfo r9=cpuid
movs r10, r5 @ invalid processor (r5=0)?

#if 0
THUMB( it eq ) @ force fixup-able long branch encoding
beq __error_p @ yes, error 'p'
#endif

I tried also to patch hard coded arguments ttyS0 in the file board-omapl138-hawk.c, function omapl138_hawk_console_init()

I will appreciate any help.

Thank you.