Other Parts Discussed in Thread: PROFIBUS, ISO1176
Hi ,
I have a custom AM335x board and i am trying to achieve rs485 master , slave communication using libmodbus library in linux.
I am using ISO1176 ISOLATED RS-485 PROFIBUS TRANSCEIVER.
And I am getting error such as "ERROR CRC received" while communicating.
So my question is.
1. As profibus is part of PRU subsystem , so does it need any special firmware ?
2. Have the AM335x profibus tested with libmodbus library in linux .?
3. If AM335x profibus not tested with libmodbus library , then which library or package should be used for AM335x profibus communication ?
Please help us to resolve this issue..!
regards
Nitesh