Hello expert.
We have customized board, base on DM385, use CBB RDK 1.5
mcfw/src_bios6/utils/src/utils.c function, Timestamp_getFreq(&cpuHz)
the return value is set at double.
e.g I set 200Mhz, but read value is 400Mhz.
is something wrong?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello expert.
We have customized board, base on DM385, use CBB RDK 1.5
mcfw/src_bios6/utils/src/utils.c function, Timestamp_getFreq(&cpuHz)
the return value is set at double.
e.g I set 200Mhz, but read value is 400Mhz.
is something wrong?
Hi Badri Narayana, thank you for your reply.
ok, but I use Utils_getCurTimeInMsec() get time is wrong.
the actual value obtained was twice,
I write a test function is attached ->
//#define USE_LINUX_API
unsigned int AUDIO_GetTimeStamp(void)
{
#if defined USE_LINUX_API
struct timeval timeval;
gettimeofday(&timeval, NULL);
return (timeval.tv_sec * 1000) + (timeval.tv_usec + 500) / 1000;
#else
return (Vcam_getCurVpssM3Time());
#endif
}
//------------------------------------------------------------------------------------------------------
Void Audio_recordMain(Void * arg)
{
int runCount = 0;
int startTime = AUDIO_GetTimeStamp();
while(1) {
runCount++;
if ((AUDIO_GetTimeStamp()-startTime) >= 1000) { // time >= 1 sec
printf("#### startTime: %d, runCount: %d\n", startTime, runCount);
runCount = 0;
startTime = AUDIO_GetTimeStamp();
}
}
}
both the linux api gettimeofday(&timeval, NULL) and Vcam_getCurVpssM3Time() to compare,
the m3Time 1sec actual was 2sec.