This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127 IPNC demo gets stuck at Camera link deletion process

Hi all,

We are trying to run IPNC_RDK  demo application for DM8127 processor. We are using it with "tri-stream" usecase. If we select "dual stream" from video setting page or "smart analytics" from live video page , the usecase should restart successfully, but its getting stuck in "camera link" deletion process.


Here is the console log for the same.

///////////////////////////////////

[m3vpss ]  125404: SCLR: Delete Done !!!

[m3video] Motion Detect Task Exit Completed

[m3vpss ]  125404: DUP   : Delete Done !!!

[m3video]  125401: ENCODE: CH-1:

 [m3video]  ENC    : Delete done !!!

[m3vpss ]  124715: SWOSD   : Delete Done !!!

[m3video]  125402: IPC_IN_M3   : Delete in progress !!!

[m3vpss ]  125417: MERGE   : Delete Done !!!

[m3video]  125402: IPC_IN_M3   : Delete Done !!!

[m3vpss ]  125418: DUP   : Delete Done !!!

[m3vpss ]  125418: DUP   : Delete Done !!!

[m3vpss ]  124718: VNF:

 [m3vpss ] VNF: Delete in progress !!!

[m3vpss ]  124718: VNF:

 [m3vpss ] VNF: Delete done !!!

[m3vpss ]  124718: CAMERA: Fields = 5870 (fps = 59, CPU Load = 23)

[m3vpss ]  124718: CAMERA: Num Resets = 0 (Avg 0 ms per reset)

[m3vpss ]  124718: CAMERA: Delete in progress !!!

CPU CurrentStatus is = 0

Error: SemWait: Invalid Semaphore handler

Error: SemRelease: Invalid Semaphore handler

 

*****************************************************************

 

    IPNC BUILD VERSION: DM8127 IPNC RDK VERSION 03.50.00.08              

 

*****************************************************************

 

./bin/ipnc_rdk_mcfw.out   VA VNF_QUALITY TRISTREAM TRIPLE_H264 TI2A AEWB 1080P_D1 H264 HIGH_SPEED1 H264 HIGH_SPEED2 MJPEG 80 &

[c6xdsp ] Remote Debug Shared Memory @ 0xbff00000

[m3video] Remote Debug Shared Memory @ 0xbff05020

[m3vpss ] Remote Debug Shared Memory @ 0xbff0a040

[c6xdsp ] Remote Debug Shared Memory @ 0xbff00000

[m3video] Remote Debug Shared Memory @ 0xbff05020

[m3vpss ] Remote Debug Shared Memory @ 0xbff0a040

[c6xdsp ] Remote Debug Shared Memory @ 0xbff00000

[m3video] Remote Debug Shared Memory @ 0xbff05020

[m3vpss ] Remote Debug Shared Memory @ 0xbff0a040

[c6xdsp ] Remote Debug Shared Memory @ 0xbff00000

[m3video] Remote Debug Shared Memory @ 0xbff05020

[m3vpss ] Remote Debug Shared Memory @ 0xbff0a040

[c6xdsp ]  133447: SYSTEM  : System DSP Init in progress !!!

[c6xdsp ]  133460: SYSTEM: Creating ListMP [DSP_IPC_OUT_23] in region 0 ...

[c6xdsp ]  133461: Assertion @ Line: 56 in links_common/system/system_ipc_listMP.c: *pOutHndl != NULL : failed !!!

[m3video]  134186: SYSTEM  : System Video Init in progress !!!

[m3video]  134186: SYSTEM  : System Video Init Done !!!

[m3video]  134187: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_0] in region 0 ...

[m3video]  134187: Assertion @ Line: 56 in links_common/system/system_ipc_listMP.c: *pOutHndl != NULL : failed !!!

ApproDrvInit: 7

Creat queue id:163844

queue id:163844

//////////////////////////////////

Please help me out to resolve this problem.

Thanks and regards,

Jay