This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debugging custom U-boot

I'm trying to port U-boot from the EVMK2H board to my own custom board based off of the K2H. I'm having issues where I'm not even seeing the U-Boot version and date string print on the console. FYI I have verified I am using the correct UART port.

I found a related page here http://processors.wiki.ti.com/index.php/Sitara_Linux_Training:_uboot_linux_debug_with_ccsv5 and I followed the steps to load symbols via Load Symbols. It shows in the bottom right that it is "Loading symbols"... but no symbols are loaded. I am loading the correct file (u-boot as opposed to the binary u-boot.bin)

Can someone help understand why the symbols aren't being loaded? 

  • Hi Justin,

    Please follow the below to download and debug the u-boot.bin in MSMC SRAM.

    http://processors.wiki.ti.com/index.php/MCSDK_UG_Chapter_Exploring#Running_U-Boot.2C_Boot_Monitor_and_Linux_Kernel_on_EVM

    Could you please provide the difference between the EVM and Custom design?

    Have you tried loading the pre-built binary from MCSDK3.x?

    Thanks.

  • The clocks on my custom design are as follows:

    - SYSCLK is 153.6 MHz
    - ARMCLK is 122.88 MHz
    - DDR3A and DDR3B are 100 MHz
    - SRIOSGMIICLK is 156.25 MHz

    Right now I am debugging the ethernet interface, in the Uboot environment. We are using the same Marvell 88E1111 PHY and SRIOSGMIICLK values in our design as the EVM. As such, I left the CONFIGs the same:

    /* Network Configuration */
    #define CONFIG_ETH_PHY_MARVEL_88E1111
    #define CONFIG_DRIVER_TI_KEYSTONE_NET
    #define CONFIG_MII
    #define CONFIG_BOOTP_DEFAULT
    #define CONFIG_BOOTP_DNS
    #define CONFIG_BOOTP_DNS2
    #define CONFIG_BOOTP_SEND_HOSTNAME
    #define CONFIG_NET_RETRY_COUNT 32
    #define CONFIG_NET_MULTI
    #define CONFIG_GET_LINK_STATUS_ATTEMPTS 5
    #define CONFIG_SYS_SGMII_REFCLK_MHZ 312
    #define CONFIG_SYS_SGMII_LINERATE_MHZ 1250
    #define CONFIG_SYS_SGMII_RATESCALE 2

    One difference is I am using the SGMII2 interface instead of 0 or 1 like the EVM. What changes might I have to make for this difference? I noticed the addition of eth2 and eth3 in eth_priv_t eth_priv_cfg[] which is in board.c and one difference is .sgmii_link_type =SGMII_LINK_MAC_MAC_FORCED versus .sgmii_link_type = SGMII_LINK_MAC_PHY. But I'm not sure what the differences between those two are in relation to my issue. Uboot seems to initialize all 4 interfaces just fine and gets to the command prompt, but if I try to do something like "ping", there is no response.

    Any thoughts on how to attack this?

  • After gaining a bit of understanding on the setup this is where I am at:

    In custom/board.c:

    eth_priv_cfg[] = {
    {
    .int_name = "K2HK_EMAC2",
    .rx_flow = 24,
    .phy_addr = 0,
    .slave_port = 3,
    .sgmii_link_type = SGMII_LINK_MAC_PHY,
    }
    }

    In ./drivers/net/keystone_net.c I changed which port reads the internal MACID:

    if (eth_priv->slave_port == 3) {
    maca = __raw_readl(MAC_ID_BASE_ADDR);
    macb = __raw_readl(MAC_ID_BASE_ADDR + 4);
    }

    So now things are looking reasonable. Let's read back the Port 3 SGMII registers:

    02090400: 4ec20101 00000000 00000000 00000000 ...N............
    02090410: 00000001 0000003d 00000001 00000000 ....=...........
    02090420: 0000d801 00000000 00000000 00000000 ................
    02090430: 00000000 00000000 00000000 00000000 ................
    02090440: 00000000 00000000 00000ee9 00000000 ................

    The MR_LP_ADV_ABILITY indicates a successful autoneg. These also match the same regs for port 0 of the EVM when it's connected.

    But when I look at the STATS regsiters is where the problem is:

    02090b00: 00000000 00000000 00000000 00000000 ................
    02090b10: 00000000 00000000 00000000 00000000 ................
    02090b20: 00000000 00000000 00000000 00000000 ................
    02090b30: 00000000 00000000 00000000 00000000 ................
    02090b40: 00000000 00000000 00000000 00000000 ................
    02090b50: 00000000 00000000 00000000 00000000 ................
    02090b60: 00000000 00000000 00000000 00000000 ................
    02090b70: 00000000 00000000 00000000 00000000 ................
    02090b80: 00000000 00000000 00000000 00000000 ................
    02090b90: 00000000 00000000 00000000 00000000 ................
    02090ba0: 00000000 00000000 00000000 00000000 ................
    02090bb0: 00000000 00000000 00000000 00000000 ................
    02090bc0: 00000000 00000000 00000000 00000000 ................
    02090bd0: 00000000 00000000 00000000 00000000 ................
    02090be0: 00000000 00000000 00000000 00000000 ................
    02090bf0: 00000000 00000000 00000000 00000000 ................
    02090c00: 00000000 00000000 00000000 00000000 ................
    02090c10: 00000000 00000000 00000000 00000000 ................
    02090c20: 00000000 00000000 00000000 00000000 ................
    02090c30: 00000000 00000000 00000000 00000000 ................
    02090c40: 00000000 00000000 00000000 00000000 ................
    02090c50: 00000000 00000000 00000000 00000000 ................
    02090c60: 00000000 00000000 00000000 00000000 ................
    02090c70: 00000000 00000000 00000000 00000000 ................
    02090c80: 00000000 00000000 00000000 00000000 ................
    02090c90: 00000000 00000000 00000000 00000000 ................
    02090ca0: 00000000 00000000 00000000 00000000 ................
    02090cb0: 00000000 00000000 00000000 00000000 ................
    02090cc0: 00000000 00000000 00000000 00000000 ................
    02090cd0: 00000000 00000000 00000000 00000000 ................
    02090ce0: 00000000 00000000 00000000 00000000 ................
    02090cf0: 00000000 00000000 00000000 00000000 ................


    There are no RX/TX STATS, after trying to ping, or dhcp, or connecting a laptop directly to the board and sending traffic.

  • Hi,

    Have you configured the the u-boot to use correct port to ping or dhcp?

    If not configure the ethact and ethaddr u-boot environment variables correctly. Then try ping or dhcp commands.

    Example for port 1:

    setenv ethact ____#1

    setenv ethaddr1 12:34:45:xx:xx:xx

  • Rajasekaran,

    Thanks for the reply. Those ARE set. 

    For what it's worth, I also enabled the POST for the post_eth_loopback_test and it comes back "FAILED".

    See debug prints:

    POST EMAC TEST for port 2 ... + emac_open
    - emac_open
    {post_eth_loopback_test}: PHY REG0=0x1140
    {post_eth_loopback_test}: PHY REG2=0x0141
    {post_eth_loopback_test}: PHY REG3=0x0CC2
    {post_eth_loopback_test}: tci6614_eth_phy_read ret=0 from phy_addr=0
    {post_eth_loopback_test}: PHY REG0=0x0140
    {post_eth_loopback_test}: writing 0x4140 to phy_addr=0
    {post_eth_loopback_test}: PHY REG0=0x4140
    {init_mac}: port=0, mac[0]=0x7C,mac[1]=0x66{init_mac}: port=1, mac[0]=0x7C,mac[1]=0x66{init_mac}: port=2, mac[0]=0x7C,mac[1]=0x66{tci6614_eth_send_packet}: loopback_test=1
    {tci6614_eth_send_packet}: Sending packet...
    {tci6614_eth_send_packet}: Returning=270
    We havn't received the packet back
    + emac_close
    - emac_close
    FAILED

    As you can see it is putting the PHY in loopback mode, and trying to send a packet, but it fails. Thanks.

  • Hi Justin,

    I have reviewed your u-boot code changes, i have a suggestion to verify at your end.

    1. Instead of having only EMAC2 configuration on eth_priv_cfg[], could you add EMAC2 configurations to the existing EMAC configuration as below and try.

    eth_priv_t eth_priv_cfg[] = {
            {
                    .int_name       = "TCI6638_EMAC",
                    .rx_flow        = 22,
                    .phy_addr       = 0,
                    .slave_port     = 1,
                    .sgmii_link_type = SGMII_LINK_MAC_PHY,
            },
    
            {
                    .int_name       = "TCI6638_EMAC1",
                    .rx_flow        = 23,
                    .phy_addr       = 1,
                    .slave_port     = 2,
                    .sgmii_link_type = SGMII_LINK_MAC_PHY,
            },
    
            {
                    .int_name       = "TCI6638_EMAC2",
                    .rx_flow        = 24,
                    .phy_addr       = 2,
                    .slave_port     = 3,
                    .sgmii_link_type = SGMII_LINK_MAC_PHY,
            },
    };
    

    2. Please try ping or dhcp with below environment variables set. I have verified this in EVM  for TCI6638_EMAC1(default it uses TCI6638_EMAC).

    setenv ethact TCI6638_EMAC2
    setenv eth2addr 11:22:33:44:55:66
    setenv ipaddr xx.xx.xx.xx
    setenv gatewayip xx.xx.xx.xx
    saveenv
    reset

  • Rajasekaran,

    Thanks for the reply. I had already put those fields back in the array because I noticed that the POST code needed it that way as it used the index into eth_priv_cfg as synonymous with the slave port number. 

    Going from a different angle. I tried the SGMII loopback test but I wasn't sure what to expect besides seeing that it showed the  Link indicator bit in SGMII 3 status as "UP".  I'm working on trying the MAC Loopback now.

    Q1. Which loopback test would you suggest to help isolate whether this is truly a software issue, or perhaps a hardware issue.

    Q2. By the way, I'm curious how the SGMII Status register showing Autonegotiation is complete and the Link Partner Advertised Ability Register (MR_LP_ADV_ABILITY) are filled if MDIO is disabled (has_mdio=0). Does this indicate that the PHY is talking to the Keystone on some level via the SGMII lines?

    Thanks.

  • This has turned into an interesting DDR3 issue instead of a SGMII Ethernet one. Please see this post: http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/340504.aspx

    The MAC and SGMII loopbacks were a good test that demonstrated it worked on the EVM but not our board with Uboot running from DDR3. Once I moved Uboot to the Shared Memory SRAM it worked just fine!

  • Hi Justin,

    Good to hear that the u-boot worked fine. 

    My very first suggestion is, to run the u-boot on SRAM. Hope to resolve the DDR issue soon.

    http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/339435/1186114.aspx#1186114

    Thank you for the update.

  • Rajasekaran , I'm sorry to reject your Verification but the original question in this post hasn't been answered. I was using the method in your link from the very beginning. I make uboot, copy the .bin into memory, use Load Symbols on the "u-boot" file, but no symbols are loaded it seems.

  • Hi Justin,

    1. Set the EVM in no boot mode.

    2. Load the target configuration file, connect to the first core of ARM and load the gel file.

    Then follow below wiki link to debug the u-boot using symbol file.

    http://processors.wiki.ti.com/index.php/Sitara_Linux_Training:_uboot_linux_debug_with_ccsv5#Perform_U-Boot_Debug

    Thanks.