Hi,
Currently, I am doing research on memory management on OMAP5. I want to know whether OMAP5 supports the Hugepage or not?
Another question is about the OMAP5 processor TLB lock mechanism. Based on official ARM Cortex-A15 Technical Reference Manual, it says "The Cortex-A15 MMU does not support the locking of TLB entries at either Level 1 or Level 2". However, on OMAP543x Technical Reference Manual, it lists the "TLB Entry Lock Mechanism" (Page 4478). Is it mean that I can lock TLB through MMU_LOCK, MMU_CAM and MMU_RAM?
Thanks!
Best Regards,
Jianan