This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

changes to the omx encode example

hello

What structure should be used for the omx encode example to access the the number of bytes generated per frame ?

Are the number of bytes allocated same to each frame while encoding using the omx example.I tried accessing the  structure field of IVDENC2_OutArg -bytesgenerated.Bbut it returns the same value each time is it right?

Thanks

  • Hi,

    IVIDENC2_OutArg->bytesGenerated is the bytesGenerated for each frame and it will vary for each framebased on I/P/B frame and the bitRate used.

    Please check encode example which comes with ezsdk.

    Ram

  • hello ram

    We intend to encode according to the followinf frame structure.ie. IPPPPPPPPPPPPPPPIPPP.

    What chnages should be made to the encode example in ezsdk so that the encoder follows the above pattern mentioned.
    Also we are using constant bitrate of 1000000 while encoding.Are any changes to the code required to set this parameter?

    Thank you

  • Hi 

    In ilClient_utils.c of encode example, in function IL_ClientSetEncodeParams,

    Please set tDynParams.videoDynamicParams.h264EncDynamicParams.videnc2DynamicParams.intraFrameInterval = 15 instead of 90. This will configure your encoder for your GOP requirements.

    RatecontrolPreset is already set as LOW_DELAY(CBR) for constant bitrate encoding

    tStaticParam.videoStaticParams.h264EncStaticParams.videnc2Params.rateControlPreset = IVIDEO_LOW_DELAY;

    Ram