I use the c6747 core of omapl137.Now ,when i build the project,i meet the problem as follow:
------------------------------ fir.pjt - Debug ------------------------------
[main.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -pdsw225 -fr"E:/graduate c6747/evmc6747/EVMC6747_BSL_RevB/evmc6747_v1/dsp/tests/dycfir/fir/Debug" -i"E:/graduate c6747/evmc6747/EVMC6747_BSL_RevB/evmc6747_v1/dsp/include" -d"_DEBUG" -mv67p -@"Debug.lkf" "main.c"
[Linking...] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -@"Debug.lkf"
<Linking>
fatal error: file "E:/graduate
c6747/evmc6747/EVMC6747_BSL_RevB/evmc6747_v1/dsp/lib/evmc6747bsl.lib<evmc674
7.obj>" specifies ISA revision "C6400+", which is not compatible with ISA
revision "C6700+" specified in a previous file or on the command line
>> Compilation failure
Build Complete,
1 Errors, 0 Warnings, 0 Remarks.
******************************************************************
I delete -l rts64plus.lib
-l ..\..\lib\evmc6747bsl.lib
in the cmd file and write evmc6747bsl.lib include path in linker of build option on ccs.
I don't understand what's the point,and how can i solve it.