Hi All,
I'm using DM8168 custom board, have 2 ADV7182 decoders connected to VIN0 and VIN1 of the processor.
I'm able to configure these two chips and able to get output (test patters) in HDMI display using saLoopBack application.
But my target is to get output in composite output of the processor i.e IOUTD pin from processor.
I'm using "/dev/video0" and "/dev/video5" as capture devices and "/dev/video1" as display device.
Few sysfs attributes are set as below in saLoopBack application to get output in HDMI display.
system ("echo 1:dvo2 > /sys/devices/platform/vpss/graphics0/nodes");
system("echo 0 > /sys/devices/platform/vpss/display0/enabled");
system ("echo 720p-60 > /sys/devices/platform/vpss/display0/mode");
system("echo 1 > /sys/devices/platform/vpss/display0/enabled");
system("echo 0 > /sys/devices/platform/vpss/display0/enabled");
system ("echo 1080p-60 > /sys/devices/platform/vpss/display0/mode");
system("echo 0 > /sys/devices/platform/vpss/graphics0/enabled");
system("echo 1 > /sys/devices/platform/vpss/display0/enabled");
system("echo 1:hdmi > /sys/devices/platform/vpss/graphics0/nodes");
Is there any sysfs configuration exists for composite out also,whatever devices used to capture and display are proper to get output in Composite out also?
Please help me to solve this issue.
Thanks and Regards,
Nithin