This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is anyone aware of a C55x AER example for an eval board that could work as a demo



I downloaded / installed the AER packages for the C55x aer_c55l_cpuv3.3_obj_17_0_0_0

After a few minor changes builds and runs on the ezDSP5535.  There is one example project in the package located here: aer_c55l_cpuv3.3_obj_17_0_0_0\packages\ti\mas\aer\test\ccsProjects\aertest_c55l_C55L_COFF

This is a test project that execises the AER code using two canned files, fe_16k.pcm and ne_pink_16k.pcm.  That's all fine and helpful, what I really need of course is something running on an eval board with actual codec input/output so I can test the algorithm in real time with our acoustics.  

I have looked through all the AER posts in this forum and of course Googled.  I have not been able to find any AER example code that will "just run" on any of the DSP eval boards C55x or C674x.

Could you point me to something ?  Of course I could spend a lot of time getting this to go on the eZdsp board, but it seems like someone must have done this... 

  • Hi Mark

    We don't have any "productized" solution that is available in broad market that allows you to demo this out of the  box. There are some in house solutions that we have provided to field teams to demo solutions to customers with NDA etc. Nothing that we can directly hand off to customers. 

    I would recommend getting in touch with your local field office, and based on the business opportunity we can see if we can engage providing you something via the field support organization

    Regards

    Mukul