This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need examples of NDK with BIOS6

Hi!

I work with DM648. I started the project with CCSv3.3 + BIOS 5.x then I moved the project to CCSv4 + BIOS 5.40 quite smoothly. Now I' trying to use BIOS6 for the same reason as Matt. I did all steps which are described in "Migrating a DSP/BIOS 5 Application to DSP/BIOS 6" but I got a problem with NDK. It seems that other parts of the project were moved without problems but for NDK I have some problems with tcf and libraries. I tried to find an example of using NDK with BIOS6 but I didn't. Does anybody know where I can find such an example.

 

Best Regards

Victor

  • Hi,

    NDK 2.1.0 (http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/ndk/2_01_00/index_FDS.html) supports BIOS6 and a reference driver (EVM6474 NDK Support Package) is provided  with network application projects ported over to BIOS6+CCSv4.

    -Marian