TI folks,
We have developed a product based on the DM814x, using:
- DM814x PG 3.0
- EZSDK 5.05.02.00
- EZSDK OMX/HDVPSS Overlay 5.05.02.00
- PSP 04.04.00.02
- Most of the Arago updates for both linux and u-boot in ti81xx-master after the v2.6.37_TI81XXPSP_04.04.00.02.patch1 tag
I need to add a second MMC card. I followed the instructions in the famous MMC.rtf doc, and it apparently worked, but this doc is quite old, and there have been MMC-related changes to the DM814x kernel since then. Is there an updated document for how to add a second MMC card to a DM814x product?
The original MMC.rtf is attached here, for reference.
Thanks,
Dan -