Hi,
I'm using DM814x & security board with RDK 4.1.0.2
I've encoded files with demo usecase 1, and then tried to play them using vlc.
I see that the speed in vlc is much faster than the real time (everyting is quicker in the playback video).
I ran the provided demo without changing parameters in the demo.
Do you have any idea why It is not played correcty ?
Thanks,
Ran