Hi, I've a board based on AM335 CPU and I'm trying to start Android.
I've got the consolle but the graphic application do not start...
I've recompiled kernel and file system with SGX support but when system start
I've this error:
sysfs: cannot create duplicate filename '/bus/platform/devices/pvrsrvkm'
It's seems that the SGX driver is not started : any idea?
Thanks
Here the start up log
>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0-00244-gcf99001-dirty (root@srv-linux01) (gccversion 4.6.x-google 20120106 (prerelease) (GCC) ) #11 Fri May 9 09:15:40 CEST 2014
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
[ 0.000000] Kernel command line: root=/dev/nfs nfsroot=11.0.0.9:/tftpboot/rootfs rw rootdelay=2 init=/init ip=11.0.0.177 console=ttyO0,115200n8 vt.global_cursor_default=0 consoleblank=0 androidboot.console=ttyO0
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 512MB = 512MB total
[ 0.000000] Memory: 509960k/509960k available, 14328k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc077f000 (7644 kB)
[ 0.000000] .init : 0xc077f000 - 0xc07d3000 ( 336 kB)
[ 0.000000] .data : 0xc07d4000 - 0xc083a430 ( 410 kB)
[ 0.000000] .bss : 0xc083a454 - 0xc098fc98 (1367 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000183] Calibrating delay loop... 548.86 BogoMIPS (lpj=2744320)
[ 0.048736] pid_max: default: 32768 minimum: 301
[ 0.048889] Security Framework initialized
[ 0.048980] Mount-cache hash table entries: 512
[ 0.049468] CPU: Testing write buffer coherency: ok
[ 0.049530] ftrace: allocating 21921 entries in 65 pages
[ 0.132263] omap_hwmod: pruss: failed to hardreset
[ 0.133209] print_constraints: dummy:
[ 0.133453] NET: Registered protocol family 16
[ 0.134796] OMAP GPIO hardware version 0.1
[ 0.136108] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.137451] omap_i2c.1: alias fck already exists
[ 0.138092] omap2_mcspi.1: alias fck already exists
[ 0.138244] omap2_mcspi.2: alias fck already exists
[ 0.138427] edma.0: alias fck already exists
[ 0.138458] edma.0: alias fck already exists
[ 0.138488] edma.0: alias fck already exists
[ 0.150543] bio: create slab <bio-0> at 0
[ 0.151702] SCSI subsystem initialized
[ 0.152740] usbcore: registered new interface driver usbfs
[ 0.152862] usbcore: registered new interface driver hub
[ 0.153045] usbcore: registered new device driver usb
[ 0.153381] registerd cppi-dma Intr @ IRQ 17
[ 0.153411] Cppi41 Init Done Qmgr-base(e087a000) dma-base(e0878000)
[ 0.153411] Cppi41 Init Done
[ 0.153442] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.153625] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.168731] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.170196] tps65910 1-002d: JTAGREVNUM 0x0
[ 0.172454] print_constraints: VRTC:
[ 0.173858] print_constraints: VIO: at 1500 mV
[ 0.176116] print_constraints: VDD1: 600 <--> 1500 mV at 1100 mV normal
[ 0.178405] print_constraints: VDD2: 600 <--> 1500 mV at 1100 mV normal
[ 0.179351] print_constraints: VDD3: 5000 mV
[ 0.180725] print_constraints: VDIG1: at 1800 mV
[ 0.182128] print_constraints: VDIG2: at 1800 mV
[ 0.183502] print_constraints: VPLL: at 1800 mV
[ 0.184906] print_constraints: VDAC: at 1800 mV
[ 0.186279] print_constraints: VAUX1: at 1800 mV
[ 0.187683] print_constraints: VAUX2: at 3300 mV
[ 0.189056] print_constraints: VAUX33: at 3300 mV
[ 0.190460] print_constraints: VMMC: at 3300 mV
[ 0.190826] tps65910 1-002d: No interrupt support, no core IRQ
[ 0.192108] Bluetooth: Core ver 2.16
[ 0.192199] NET: Registered protocol family 31
[ 0.192199] Bluetooth: HCI device and connection manager initialized
[ 0.192230] Bluetooth: HCI socket layer initialized
[ 0.192230] Bluetooth: L2CAP socket layer initialized
[ 0.192291] Bluetooth: SCO socket layer initialized
[ 0.192840] cfg80211: Calling CRDA to update world regulatory domain
[ 0.193786] Switching to clocksource gp timer
[ 0.215850] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.216064] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.216278] MUSB0 controller's USBSS revision = 4ea20800
[ 0.216308] musb0: Enabled SW babble control
[ 0.217315] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using DMA, IRQ 18
[ 0.217559] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.217742] MUSB1 controller's USBSS revision = 4ea20800
[ 0.217773] musb1: Enabled SW babble control
[ 0.218292] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.218444] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.218597] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.218627] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.218627] usb usb1: Product: MUSB HDRC host driver
[ 0.218658] usb usb1: Manufacturer: Linux 3.2.0-00244-gcf99001-dirty musb-hcd
[ 0.218658] usb usb1: SerialNumber: musb-hdrc.1
[ 0.219268] hub 1-0:1.0: USB hub found
[ 0.219299] hub 1-0:1.0: 1 port detected
[ 0.219848] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using DMA, IRQ 19
[ 0.220245] NET: Registered protocol family 2
[ 0.220458] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.220916] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[ 0.221313] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.221527] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.221557] TCP reno registered
[ 0.221557] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.221588] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.221862] NET: Registered protocol family 1
[ 0.222198] RPC: Registered named UNIX socket transport module.
[ 0.222198] RPC: Registered udp transport module.
[ 0.222229] RPC: Registered tcp transport module.
[ 0.222229] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.222534] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.375518] ashmem: initialized
[ 0.375854] VFS: Disk quotas dquot_6.5.2
[ 0.375915] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.376953] fuse init (API version 7.17)
[ 0.377227] msgmni has been set to 996
[ 0.378540] io scheduler noop registered
[ 0.378570] io scheduler deadline registered
[ 0.378631] io scheduler cfq registered (default)
[ 0.379302] Could not set LED4 to fully on
[ 0.380737] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 1.080932] console [ttyO0] enabled
[ 1.085083] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 1.092834] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 1.100616] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 1.108337] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 1.116119] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 1.123992] [drm] Initialized drm 1.1.0 20060810
[ 1.136535] brd: module loaded
[ 1.143615] loop: module loaded
[ 1.147186] i2c-core: driver [tsl2550] using legacy suspend method
[ 1.153656] i2c-core: driver [tsl2550] using legacy resume method
[ 1.160125] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.224426] No daughter card found on AM335x EVM
[ 1.229309] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.244537] Board name: A335COOP
[ 1.247894] Board version: 00A2
[ 1.251190]
[ 1.251190] >>>>The board is a COOP-ODBC<<<<
[ 1.257812] Setup COOM-ODBC lcdc pin mux
[ 1.262329] da8xx_lcdc.0: alias fck already exists
[ 1.267730] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel
[ 1.287902] mmc0_init: COOPODBC mode (no CD, no WR)
[ 1.293182] omap_hsmmc.0: alias fck already exists
[ 1.298522] omap_hsmmc.1: alias fck already exists
[ 1.303802] <evm_nand_init: COOPODBC config GPMC bus NAND+FPGA>
[ 1.310546] omap-gpmc omap-gpmc: GPMC revision 6.0
[ 1.315582] Registering NAND on CS0
[ 1.319641] <Configure Uart1 Bluetooth pins...>
[ 1.324493] <COOPODBC: Configure Bluetooth Enable pin>
[ 1.329895] <wl12xx_bluetooth_enable: btwilink>
[ 1.334655] am335xevm: bt init
[ 1.338500] <sgx_init: am33xx_gpu_init>
[ 1.343139]
[ 1.343139] >>>>End COOP-ODBC setup <<<<
**********************************************************************
[ 1.350494] (stk) : gpio 117 request failed
[ 1.354827] kim: probe of kim failed with error -16
**********************************************************************
[ 1.360168] (hci_tty): inside hci_tty_init
[ 1.364685] (hci_tty): allocated 251, 0
[ 1.369354] NFC Driver for TI WiLink
[ 1.373992] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.381286] omap2-nand driver initializing
[ 1.385925] ONFI flash detected
[ 1.389343] ONFI param page 0 valid
[ 1.393005] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G08ABAFAWP)
[ 1.402008] Creating 8 MTD partitions on "omap2-nand.0":
[ 1.407623] 0x000000000000-0x000000020000 : "SPL"
[ 1.413848] 0x000000020000-0x000000040000 : "SPL.backup1"
[ 1.420532] 0x000000040000-0x000000060000 : "SPL.backup2"
[ 1.427246] 0x000000060000-0x000000080000 : "SPL.backup3"
[ 1.433929] 0x000000080000-0x000000260000 : "U-Boot"
[ 1.440948] 0x000000260000-0x000000280000 : "U-Boot Env"
[ 1.447601] 0x000000280000-0x000000780000 : "Kernel"
[ 1.455932] 0x000000780000-0x000010000000 : "File System"
[ 1.567077] OneNAND driver initializing
[ 1.614440] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.620910] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
[ 1.628326] davinci_mdio.0: probed
[ 1.631866] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720
[ 1.640533] PPP generic driver version 2.4.2
[ 1.645263] PPP BSD Compression module registered
[ 1.650177] PPP Deflate Compression module registered
[ 1.655639] usbcore: registered new interface driver cdc_ether
[ 1.661804] usbcore: registered new interface driver cdc_eem
[ 1.667846] usbcore: registered new interface driver dm9601
[ 1.673736] usbcore: registered new interface driver cdc_subset
[ 1.679992] cdc_ncm: 04-Aug-2011
[ 1.683441] usbcore: registered new interface driver cdc_ncm
[ 1.689483] usbcore: registered new interface driver cdc_acm
[ 1.695404] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 1.703796] Initializing USB Mass Storage driver...
[ 1.709045] usbcore: registered new interface driver usb-storage
[ 1.715332] USB Mass Storage support registered.
[ 1.720336] usbcore: registered new interface driver usbserial
[ 1.726531] USB Serial support registered for generic
[ 1.924468] usb 1-1: new full-speed USB device number 2 using musb-hdrc
[ 2.044464] usb 1-1: device descriptor read/64, error -71
[ 2.274475] usb 1-1: device descriptor read/64, error -71
[ 2.504486] usb 1-1: new full-speed USB device number 3 using musb-hdrc
[ 2.624481] usb 1-1: device descriptor read/64, error -71
[ 2.854461] usb 1-1: device descriptor read/64, error -71
[ 3.084472] usb 1-1: new full-speed USB device number 4 using musb-hdrc
[ 3.504486] usb 1-1: device not accepting address 4, error -71
[ 3.624481] usb 1-1: new full-speed USB device number 5 using musb-hdrc
[ 4.044464] usb 1-1: device not accepting address 5, error -71
[ 4.050567] hub 1-0:1.0: unable to enumerate USB device on port 1
[ 4.057098] usbcore: registered new interface driver usbserial_generic
[ 4.063934] usbserial: USB Serial Driver core
[ 4.068572] USB Serial support registered for GSM modem (1-port)
[ 4.075073] usbcore: registered new interface driver option
[ 4.080902] option: v0.7.2:USB Driver for GSM modems
[ 4.088134] gadget: Mass Storage Function, version: 2009/09/11
[ 4.094329] gadget: Number of LUNs=1
[ 4.098236] lun0: LUN: removable file: (no medium)
[ 4.103637] gadget: android_usb ready
[ 4.107604] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 4.113220] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[ 4.121093] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 4.128234] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 4.135803] usb usb2: Product: MUSB HDRC host driver
[ 4.140991] usb usb2: Manufacturer: Linux 3.2.0-00244-gcf99001-dirty musb-hcd
[ 4.148468] usb usb2: SerialNumber: musb-hdrc.0
[ 4.153839] hub 2-0:1.0: USB hub found
[ 4.157806] hub 2-0:1.0: 1 port detected
[ 4.162933] mousedev: PS/2 mouse device common for all mice
[ 4.169647] input: ti-tsc as /devices/platform/omap/ti_tscadc/tsc/input/input0
[ 4.178558] using rtc device, am33xx-rtc, for alarms
[ 4.183624] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[ 4.190979] i2c /dev entries driver
[ 4.194915] Linux video capture interface: v2.00
[ 4.200134] usbcore: registered new interface driver uvcvideo
[ 4.206176] USB Video Class driver (1.1.1)
[ 4.226928] input: lm75-temp as /devices/virtual/input/input1
[ 4.233459] lm75 1-004c: hwmon0: sensor 'lm75'
[ 4.239379] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 4.245971] device-mapper: uevent: version 1.0.3
[ 4.251037] device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-devel@redhat.com
[ 4.259918] Bluetooth: HCI UART driver ver 2.2
[ 4.264587] Bluetooth: HCI H4 protocol initialized
[ 4.269592] Bluetooth: HCILL protocol initialized
[ 4.278900] cpuidle: using governor ladder
[ 4.283386] cpuidle: using governor menu
[ 4.291229] usbcore: registered new interface driver usbhid
[ 4.297149] usbhid: USB HID core driver
[ 4.301666] logger: created 256K log 'log_main'
[ 4.306579] logger: created 256K log 'log_events'
[ 4.311645] logger: created 256K log 'log_radio'
[ 4.316619] logger: created 256K log 'log_system'
[ 4.322204] tiadc tiadc: attached adc driver
[ 4.326782] oprofile: hardware counters not available
[ 4.332092] oprofile: using timer interrupt.
[ 4.336791] Netfilter messages via NETLINK v0.30.
[ 4.341857] nf_conntrack version 0.5.0 (7968 buckets, 31872 max)
[ 4.348602] ctnetlink v0.93: registering with nfnetlink.
[ 4.354278] NF_TPROXY: Transparent proxy support initialized, version 4.1.0
[ 4.361633] NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
[ 4.368133] xt_time: kernel timezone is -0000
[ 4.372985] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 4.378814] arp_tables: (C) 2002 David S. Miller
[ 4.383758] TCP cubic registered
[ 4.387359] NET: Registered protocol family 10
[ 4.392913] Mobile IPv6
[ 4.395599] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 4.401489] IPv6 over IPv4 tunneling driver
[ 4.406585] NET: Registered protocol family 17
[ 4.411315] NET: Registered protocol family 15
[ 4.416473] Bluetooth: RFCOMM TTY layer initialized
[ 4.421630] Bluetooth: RFCOMM socket layer initialized
[ 4.427062] Bluetooth: RFCOMM ver 1.11
[ 4.430999] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 4.436614] Bluetooth: BNEP filters: protocol multicast
[ 4.442108] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 4.448516] Registering the dns_resolver key type
[ 4.453521] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 4.461639] ThumbEE CPU extension supported.
[ 4.466217] mux: Failed to setup hwmod io irq -22
[ 4.471923] Power Management for AM33XX family
[ 4.476837] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 4.483581] Copied the M3 firmware to UMEM
[ 4.488006] Cortex M3 Firmware Version = 0x181
[ 4.496795] clock: disabling unused clocks to save power
[ 4.503997] Detected MACID=1c:ba:8c:f7:e1:2a
[ 4.509918] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
[ 4.522247] net eth0: CPSW phy found : id is : 0x7c0f1
[ 4.528503] PHY 0:01 not found
[ 4.538909] ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 4.626586] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 4.638977] mmc0: new high speed SDHC card at address aaaa
[ 4.645263] mmcblk0: mmc0:aaaa SU08G 7.40 GiB
[ 4.651855] mmcblk0: p1 p2
[ 4.769165] mmc1: card claims to support voltages below the defined range. These will be ignored.
[ 4.788391] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
[ 4.795104] mmc1: new SDIO card at address 0001
[ 7.515655] PHY: 0:00 - Link is Up - 100/Full
[ 7.525299] ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 7.545104] IP-Config: Guessing netmask 255.0.0.0
[ 7.550262] IP-Config: Complete:
[ 7.553649] device=eth0, addr=11.0.0.177, mask=255.0.0.0, gw=255.255.255.255,
[ 7.561614] host=11.0.0.177, domain=, nis-domain=(none),
[ 7.567687] bootserver=255.255.255.255, rootserver=11.0.0.9, rootpath=
[ 7.575653] Waiting 2sec before mounting root device...
[ 9.592132] VFS: Mounted root (nfs filesystem) on device 0:14.
[ 9.598876] Freeing init memory: 336K
[ 9.634918] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
[ 9.886291] init: cannot open '/initlogo.rle'
[ 11.570251] init: cannot find '/system/bin/rild', disabling 'ril-daemon'
[ 11.584136] init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
[ 11.833129] android_usb: already disabled
[ 11.837768] mtp_bind_config
[ 11.840759] adb_bind_config
[ 12.479309] adb_open
****************************************************************************
root@android:/ # [ 14.047698] Disabling lock debugging due to kernel taint
[ 14.086273] ------------[ cut here ]------------
[ 14.091552] WARNING: at fs/sysfs/dir.c:481 sysfs_add_one+0x98/0xb8()
[ 14.098297] sysfs: cannot create duplicate filename '/bus/platform/devices/pvrsrvkm'
[ 14.106445] Modules linked in: pvrsrvkm(O+)
[ 14.110870] Backtrace:
[ 14.113464] [<c00176e8>] (dump_backtrace+0x0/0x114) from [<c05a8cec>] (dump_stack+0x20/0x24)
[ 14.122375] r6:000001e1 r5:c0133454 r4:de01dd30 r3:c07fcb20
[ 14.128387] [<c05a8ccc>] (dump_stack+0x0/0x24) from [<c00440d4>] (warn_slowpath_common+0x5c/0x74)
[ 14.137756] [<c0044078>] (warn_slowpath_common+0x0/0x74) from [<c00441a8>] (warn_slowpath_fmt+0x40/0x48)
[ 14.147735] r8:00000001 r7:de2ac000 r6:de2ab6d0 r5:de2ac000 r4:ffffffef
[ 14.154632] r3:00000009
[ 14.157440] [<c0044168>] (warn_slowpath_fmt+0x0/0x48) from [<c0133454>] (sysfs_add_one+0x98/0xb8)
[ 14.166778] r3:de2ac000 r2:c06ed8d0
[ 14.170562] [<c01333bc>] (sysfs_add_one+0x0/0xb8) from [<c0133d70>] (sysfs_do_create_link+0x108/0x1f4)
[ 14.180389] r7:df013db0 r6:de2ab7c0 r5:de01dd88 r4:de2ab6d0
[ 14.186370] [<c0133c68>] (sysfs_do_create_link+0x0/0x1f4) from [<c0133e78>] (sysfs_create_link+0x1c/0x20)
[ 14.196472] [<c0133e5c>] (sysfs_create_link+0x0/0x20) from [<c02d57fc>] (bus_add_device+0xd4/0x180)
[ 14.206054] [<c02d5728>] (bus_add_device+0x0/0x180) from [<c02d3c58>] (device_add+0x470/0x590)
[ 14.215118] r8:c0881774 r7:00000000 r6:c081dca0 r5:bf021d20 r4:bf021d18
[ 14.222015] r3:00000000
[ 14.224792] [<c02d37e8>] (device_add+0x0/0x590) from [<c02d7df4>] (platform_device_add+0x108/0x1b8)
[ 14.234344] [<c02d7cec>] (platform_device_add+0x0/0x1b8) from [<c02d816c>] (platform_device_register+0x30/0x34)
[ 14.244964] r7:00000001 r6:00000000 r5:00000000 r4:bf021d10
[ 14.251129] [<c02d813c>] (platform_device_register+0x0/0x34) from [<bf02e074>] (PVRCore_Init+0x74/0x158 [pvrsrvkm])
[ 14.262145] r4:bf0222d0 r3:c02d77d8
[ 14.265991] [<bf02e000>] (PVRCore_Init+0x0/0x158 [pvrsrvkm]) from [<c0008780>] (do_one_initcall+0x124/0x18c)
[ 14.276336] r6:00000000 r5:c083a480 r4:de01c000
[ 14.281250] [<c000865c>] (do_one_initcall+0x0/0x18c) from [<c0077cf8>] (sys_init_module+0x3ec/0x1bd8)
[ 14.290985] [<c007790c>] (sys_init_module+0x0/0x1bd8) from [<c00138e0>] (ret_fast_syscall+0x0/0x30)
[ 14.300537] ---[ end trace 24b1ab72fe08700f ]---
[ 14.481475] omaplfb: Unknown symbol PVRGetDisplayClassJTable (err 0)
[ 14.893676] init: untracked pid 73 exited
root@android:/ # [ 17.931030] init: untracked pid 134 exited
****************************************************************************
root@android:/ #