This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[Omap L138] High Speed USB problem

Hi All,


   My application need the USB to be in device mode only and i have set it up as a pure device mode without OTG. However, it high speed negotiation is enable, the host PC will detect the device as "unknown device". If i disable the high speed, it will work in full speed and device can be recognize by the PC.

  Do you guys has any idea what is wrong?

  I have tried using another cable, but the result is the same. ( the cable i has is about 50m long).

Regards,

Tom