DDR is not used in our design, how to handle the DDRREFCLK (N/P)? The DSP Hardware Design Guide provides two conflict handlings.
-
- On pg8, LJCB(Low Jitter Clock Buffer) should handle as Fig 3, which state that LJCB_P connect to 1.1V and LJCB_N connect 1Kohm resistor to GND
- On pg34, it state that: If the DDR2 peripheral is disabled, all interface signals (including reference clocks) can be left floating and input buffers will be powered down.
Thanks.