This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error on "build MAD image"

 

 

Hello.

 

I tried to make MAD image with sample that is "image_processing".

But I met an error. So I ask you to help.

 

I used compiler ver7.4.4 (C:\ti\ccsv5\tools\compiler\c6000_7.4.4)

And I use python27.

Thus, I modified the batch file like below. (C:\ti\mcsdk_2_01_02_06\demos\image_processing\utils\mad\evmc6670l\build_mad_image.bat)

@set PATH="C:\ti\ccsv5\tools\compiler\c6000_7.4.4\bin";%PATH%

@rd /s /q tmp

c:\python27\python ..\..\..\..\..\tools\boot_loader\mad-utils\map-tool\maptool.py config-files\maptoolCfg_evmc6670l.json

 

Then, I started to build MAD image

->   

C:\ti\mcsdk_2_01_02_06\demos\image_processing\utils\mad\evmc6670l>build_mad_image.bat

C:\ti\mcsdk_2_01_02_06\demos\image_processing\utils\mad\evmc6670l>c:\python27\python ..\..\..\..\..\tools\boot_loader\mad-utils\map-tool\maptool.py config-files\maptoolCfg_evmc6670l.json

C:\ti\mcsdk_2_01_02_06\demos\image_processing\utils\mad\evmc6670l>"strip6x" -o=./tmp/strippedImages\master.strip ./images/appImages\master

C:\ti\mcsdk_2_01_02_06\demos\image_processing\utils\mad\evmc6670l>"strip6x" -o=./tmp/strippedImages\slave.strip ./images/appImages\slave

 ...

C:\ti\mcsdk_2_01_02_06\demos\image_processing\utils\mad\evmc6670l>"prelink6x" c:\users\admin\appdata\local\temp\tmp5qxxch\prelink.cmd
error: input object file, 'c:\users\admin\appdata\local\temp\tmp5qxxch\master',   is not dynamic
"c:\users\admin\appdata\local\temp\tmp5qxxch\master", line 1: error: illegal   input character: '0x7f'
"c:\users\admin\appdata\local\temp\tmp5qxxch\master", line 1: error: illegal   input character: '"'"'
"c:\users\admin\appdata\local\temp\tmp5qxxch\master", line 3: error: illegal   input character: '0x7'
"c:\users\admin\appdata\local\temp\tmp5qxxch\master", line 3: error: illegal   input character: '0xffffffc7'
"c:\users\admin\appdata\local\temp\tmp5qxxch\master", line 10: error: invalid   option:
   -c€Z.d€0d€#0P€?g€60€<0i€H0€Z0k€_0k€k0€}0n€?o€?€?q€?P€?s€?F€?u€
   0u€?F€?x€?F€?z€?{€1{€
"c:\users\admin\appdata\local\temp\tmp5qxxch\master", line 15: error: invalid   option: -equiv=content-type
fatal error: cannot find file:  FileExt
ERROR: Prelinker run pass-1 failed   <= error at prelinker

 

Please help me to make MAD image with sample.