This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x PHY 0:01 not found

Other Parts Discussed in Thread: AM3358

Hi

   I am using the am3358.The produce has two ethernet ports.The SDK version is ti-sdk-am335x-evm-05.05.00.When i modified the linux code.The two ethernet port can work.But when the system is reset,it often don't work.the log is like this:

U-Boot SPL 2011.09 (Apr 17 2014 - 05:04:56)
Texas Instruments Revision detection unimplemented


U-Boot 2011.09 (Apr 17 2014 - 05:04:56)

I2C:   ready
DRAM:  256 MiB
WARNING: Caches not enabled
NAND:  HW ECC Hamming Code selected
128 MiB
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
Net:   cpsw
Hit any key to stop autoboot:  0
Card did not respond to voltage select!
Booting from nand ...
HW ECC BCH8 Selected

NAND read: device 0 offset 0x280000, size 0x500000
 5242880 bytes read: OK
## Booting kernel from Legacy Image at 80007fc0 ...
   Image Name:   Linux-3.2.0
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2693216 Bytes = 2.6 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   XIP Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[    0.000000] Linux version 3.2.0 (mxz@ubuntu) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #6 Thu Apr 17 04:37:25 PDT 2014
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: am335xevm
[    0.000000] Memory policy: ECC disabled, Data cache writeback
[    0.000000] AM335X ES1.0 (sgx neon )
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024
[    0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=7,2048 noinitrd rootfstype=ubifs rootwait=1 ip=none
[    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[    0.000000] Memory: 256MB = 256MB total
[    0.000000] Memory: 254244k/254244k available, 7900k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xd0800000 - 0xff000000   ( 744 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
[    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)
[    0.000000]       .text : 0xc0008000 - 0xc04be000   (4824 kB)
[    0.000000]       .init : 0xc04be000 - 0xc04f9000   ( 236 kB)
[    0.000000]       .data : 0xc04fa000 - 0xc054ef28   ( 340 kB)
[    0.000000]        .bss : 0xc054ef4c - 0xc057aae4   ( 175 kB)
[    0.000000] NR_IRQS:396
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[    0.000000] Total of 128 interrupts on 1 active controller
[    0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[    0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[    0.000000] Console: colour dummy device 80x30
[    0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[    0.058959] pid_max: default: 32768 minimum: 301
[    0.059082] Security Framework initialized
[    0.059173] Mount-cache hash table entries: 512
[    0.059539] CPU: Testing write buffer coherency: ok
[    0.079406] omap_hwmod: pruss: failed to hardreset
[    0.080474] print_constraints: dummy:
[    0.080841] NET: Registered protocol family 16
[    0.082946] OMAP GPIO hardware version 0.1
[    0.085266] omap_mux_init: Add partition: #1: core, flags: 0
[    0.087280] dan_SD card pin init end
[    0.087371]  omap_hsmmc.0: alias fck already exists
[    0.087677] rmii1_init
[    0.087707] _omap_mux_get_by_name: Could not find signal gpmc_csn3.rmii2_crs_dv
[    0.087799] rmii2_init
[    0.088592] am33xx_cpsw_init,mac:20:cd:39:d9:87:4b
[    0.089996]  edma.0: alias fck already exists
[    0.090026]  edma.0: alias fck already exists
[    0.090026]  edma.0: alias fck already exists
[    0.108215] bio: create slab <bio-0> at 0
[    0.110443] SCSI subsystem initialized
[    0.112884] Switching to clocksource gp timer
[    0.128234] NET: Registered protocol family 2
[    0.128417] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.128723] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[    0.128875] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[    0.128967] TCP: Hash tables configured (established 8192 bind 8192)
[    0.128997] TCP reno registered
[    0.128997] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.129028] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.129211] NET: Registered protocol family 1
[    0.129486] RPC: Registered named UNIX socket transport module.
[    0.129486] RPC: Registered udp transport module.
[    0.129486] RPC: Registered tcp transport module.
[    0.129516] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.129730] NetWinder Floating Point Emulator V0.97 (double precision)
[    0.129974] omap-gpmc omap-gpmc: GPMC revision 6.0
[    0.129974] Registering NAND on CS0
[    0.141571] VFS: Disk quotas dquot_6.5.2
[    0.141632] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.142181] msgmni has been set to 496
[    0.145355] alg: No test for stdrng (krng)
[    0.146057] io scheduler noop registered
[    0.146057] io scheduler deadline registered
[    0.146118] io scheduler cfq registered (default)
[    0.147857] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[    0.569610] console [ttyO0] enabled
[    0.573822] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[    0.581634] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[    0.589416] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[    0.597198] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[    0.604980] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[    0.621887] brd: module loaded
[    0.629943] loop: module loaded
[    0.633422] i2c-core: driver [tsl2550] using legacy suspend method
[    0.639892] i2c-core: driver [tsl2550] using legacy resume method
[    0.647827] mtdoops: mtd device (mtddev=name/number) must be supplied
[    0.654968] omap2-nand driver initializing
[    0.659545] ONFI flash detected
[    0.662933] ONFI param page 0 valid
[    0.666625] NAND device: Manufacturer ID: 0x01, Chip ID: 0xf1 (AMD S34ML01G1)
[    0.674285] Creating 8 MTD partitions on "omap2-nand.0":
[    0.679809] 0x000000000000-0x000000020000 : "SPL"
[    0.686157] 0x000000020000-0x000000040000 : "SPL.backup1"
[    0.693054] 0x000000040000-0x000000060000 : "SPL.backup2"
[    0.700012] 0x000000060000-0x000000080000 : "SPL.backup3"
[    0.706939] 0x000000080000-0x000000260000 : "U-Boot"
[    0.714050] 0x000000260000-0x000000280000 : "U-Boot Env"
[    0.720794] 0x000000280000-0x000000780000 : "Kernel"
[    0.729217] 0x000000780000-0x000008000000 : "File System"
[    0.786010] OneNAND driver initializing
[    0.790679] UBI: attaching mtd7 to ubi0
[    0.794708] UBI: physical eraseblock size:   131072 bytes (128 KiB)
[    0.801239] UBI: logical eraseblock size:    126976 bytes
[    0.806884] UBI: smallest flash I/O unit:    2048
[    0.811767] UBI: sub-page size:              512
[    0.816589] UBI: VID header offset:          2048 (aligned 2048)
[    0.822845] UBI: data offset:                4096
[    1.848175] UBI: max. sequence number:       57
[    1.866729] UBI: attached mtd7 to ubi0
[    1.870635] UBI: MTD device name:            "File System"
[    1.876403] UBI: MTD device size:            120 MiB
[    1.881561] UBI: number of good PEBs:        964
[    1.886383] UBI: number of bad PEBs:         0
[    1.891021] UBI: number of corrupted PEBs:   0
[    1.895660] UBI: max. allowed volumes:       128
[    1.900451] UBI: wear-leveling threshold:    4096
[    1.905364] UBI: number of internal volumes: 1
[    1.910003] UBI: number of user volumes:     1
[    1.914611] UBI: available PEBs:             0
[    1.919250] UBI: total number of reserved PEBs: 964
[    1.924346] UBI: number of PEBs reserved for bad PEB handling: 9
[    1.930603] UBI: max/mean erase counter: 2/0
[    1.935058] UBI: image sequence number:  1794978710
[    1.940246] UBI: background thread "ubi_bgt0d" started, PID 456
[    1.947052] CAN device driver interface
[    1.951049] CAN bus driver for Bosch D_CAN controller 1.0
[    2.003540] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[    2.009979] davinci_mdio davinci_mdio.0: detected phy mask fffffff6
[    2.017761] davinci_mdio.0: probed
[    2.021301] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
[    2.028656] davinci_mdio davinci_mdio.0: phy[3]: device 0:03, driver unknown
[    2.036621] mousedev: PS/2 mouse device common for all mice
[    2.043395] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
[    2.050079] omap_rtc: already running
[    2.054077] i2c /dev entries driver
[    2.058685] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    2.065246] _regulator_get: deviceless supply vdd_mpu not found, using dummy regulator
[    2.073944] cpuidle: using governor ladder
[    2.078674] cpuidle: using governor menu
[    2.084747] omap4_aes_mod_init: loading AM33X AES driver
[    2.090393] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[    2.096923] omap4_aes_probe: probe() done
[    2.101318] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[    2.107452] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[    2.118957] omap4_sham_probe: probe() done
[    2.123626] oprofile: hardware counters not available
[    2.128906] oprofile: using timer interrupt.
[    2.133361] nf_conntrack version 0.5.0 (3972 buckets, 15888 max)
[    2.140106] ip_tables: (C) 2000-2006 Netfilter Core Team
[    2.145782] TCP cubic registered
[    2.149169] NET: Registered protocol family 17
[    2.153808] can: controller area network core (rev 20090105 abi 8)
[    2.160369] NET: Registered protocol family 29
[    2.165008] can: raw protocol (rev 20090105)
[    2.169464] can: broadcast manager protocol (rev 20090105 t)
[    2.175415] Registering the dns_resolver key type
[    2.180358] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[    2.188354] ThumbEE CPU extension supported.
[    2.192871] mux: Failed to setup hwmod io irq -22
[    2.198394] Power Management for AM33XX family
[    2.203216] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[    2.209899] Copied the M3 firmware to UMEM
[    2.214752] sr_init: platform driver register failed
[    2.223297] clock: disabling unused clocks to save power
[    2.241302] Detected MACID=20:cd:39:d9:87:4b
[    2.246795] cpsw: Detected MACID = 20:cd:39:d9:87:4d
[    2.253021] omap_rtc omap_rtc: setting system clock to 2012-07-27 10:40:41 UTC (1343385641)
[    2.403961] UBIFS: mounted UBI device 0, volume 0, name "rootfs"
[    2.410247] UBIFS: file system size:   119357440 bytes (116560 KiB, 113 MiB, 940 LEBs)
[    2.418518] UBIFS: journal size:       9023488 bytes (8812 KiB, 8 MiB, 72 LEBs)
[    2.426147] UBIFS: media format:       w4/r0 (latest is w4/r0)
[    2.432220] UBIFS: default compressor: lzo
[    2.436492] UBIFS: reserved for root:  0 bytes (0 KiB)
[    2.444061] VFS: Mounted root (ubifs filesystem) on device 0:12.
[    2.450653] Freeing init memory: 236K
INIT: version 2.86 booting
Please wait: booting...
Starting udev
Error opening /dev/fb0: No such device
[    4.136199] alignment: ignoring faults is unsafe on this CPU.  Defaulting to fixup mode.
Root filesystem already rw, not remounting
Caching udev devnodes
logger: mount: mount point /proc/bus/usb does not exist
ALSA: Restoring mixer settings...
Configuring network interfaces... /usr/sbin/alsactl: load_state:1625: No soundcards found...
[    4.830352] PHY 0:01 not found
udhcpc (v1.13.2) started
Sending discover...
Sending discover...
Sending discover...
No lease, forking to background
done.
Setting up IP spoofing protection: rp_filter.
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.

can you help me