This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP5: DPI to HDMI Encoder driver for TDF19988

Hi,

Is there DPI to HDMI encoder (i.e. TDF19988) driver available for OMAP5/Linux somewhere or is there any plan to support this? or Is there any sample driver available which I can use to write one for this? I am trying to bring up second display which is connected via DPI to TDF19988 for HDMI on OMAP5 ES2.0/linux3.4.25 based platform?

Regards,

Vikash

  • Hi Vikash,

    Unfortunately there is no information if there will be supported driver in the near future.

    As from the looks of it you might be the only one who will successfully port it.

    http://comments.gmane.org/gmane.comp.video.dri.devel/105551

    Regards,

    Boyko