This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Building Android ICS for beagleboardXM

Hi All,

I'm trying to build TI-Android-ICS-4.0.3_AM37x_3.0.0 for beagleboardXM. However, I am facing this issue "make[1]: *** [kernel/bounds.s] Error 1" when trying to build the kernel

Clean step

root@val-pc:~/rowboat-android/TI-Android-ICS-4.0.3_AM37x_3.0.0/kernel# make ARCH=arm CROSS_COMPILE=arm-eabi- distclean
  CLEAN   .tmp_versions
  CLEAN   scripts/basic
  CLEAN   scripts/kconfig
  CLEAN   include/config include/generated
  CLEAN   .config include/linux/version.h

Configuring step

root@val-pc:~/rowboat-android/TI-Android-ICS-4.0.3_AM37x_3.0.0/kernel# make ARCH=arm CROSS_COMPILE=arm-eabi- omap3_beagle_android_defconfig
  HOSTCC  scripts/basic/fixdep
  HOSTCC  scripts/basic/docproc
  HOSTCC  scripts/kconfig/conf.o
  HOSTCC  scripts/kconfig/kxgettext.o
  SHIPPED scripts/kconfig/zconf.tab.c
  SHIPPED scripts/kconfig/lex.zconf.c
  SHIPPED scripts/kconfig/zconf.hash.c
  HOSTCC  scripts/kconfig/zconf.tab.o
  HOSTLD  scripts/kconfig/conf
#
# configuration written to .config
#

Building step

root@val-pc:~/rowboat-android/TI-Android-ICS-4.0.3_AM37x_3.0.0/kernel# make ARCH=arm CROSS_COMPILE=arm-eabi- uImage
scripts/kconfig/conf --silentoldconfig Kconfig
  CHK     include/linux/version.h
  UPD     include/linux/version.h
  CHK     include/generated/utsrelease.h
  UPD     include/generated/utsrelease.h
  Generating include/generated/mach-types.h
  CC      kernel/bounds.s
arm-eabi-gcc: Internal error: Killed (program cc1)
Please submit a full bug report.
See <http://gcc.gnu.org/bugs.html> for instructions.
make[1]: *** [kernel/bounds.s] Error 1
make: *** [prepare0] Error 2

PATH variable

root@val-pc:~/rowboat-android/TI-Android-ICS-4.0.3_AM37x_3.0.0/kernel# echo $PATH
/root/rowboat-android/TI-Android-ICS-4.0.3_AM37x_3.0.0/prebuilt/linux-x86/toolchain/arm-eabi-4.4.3/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games


Any help will be appreciated.

Regards,

Joseph