Hi all
I use DM8168 EVM , dvrrdk4.1
the captureLink capture two channels 1080I@60. Dei_0 use SYSTEM_LINK_ID_DEI_HQ_0. Dei_1 use SYSTEM_LINK_ID_DEI_0.
I use Dei_0 as deinterlace(1080i->1080P). Dei_1 as downscale, 1080P->d1
I set Dei_0 work at EOE mode.
after Dei_1, finially will pass to DSP ,now just use nullLink as test.
Now in this chain, the Dei_1 is always skip frames , because the pFrame->fid didn't equal to nextFid.