Hi All,
Recently I received a backplane to connect 3 dm816x devices (1 master & 2 slaves). The connection is through PCIe and also has a PEX 8615 Switch.
If I use al the values in the DIP Switch to 0's the master lanes are connected, but only the master appear when I do lspci. However, when I use the default configuration in the DIP Switch, the lanes of both slaves are connected, but not the master's. Also, when I do lspci, nothing appears.
If anybody have solved this problem or has similar ones, tricks or any advice would be glad to know.
BR,
Inigo