This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2S timing requirements and CLKPOL indication when in DSP format mode

Hello, the C5505 I2S user guide indicates that the sampling / clocking edges of the I2S data is a function of both the CLKPOL and FRMT bits in the I2SSCTRL register. It appears that the timing requirement descriptions indicated in the C5505 datasheet which reference a given CLKPOL value may only be correct when FRMT=0 (I2S mode). When FRMT = 1 (DSP mode), the descriptions appear to be inverted.

If this is the case, which are the correct parameters to use for the frame sync signal timing requirements 9 and 10 when CLKPOL = 0 and FRMT = 1? My implementation matches that described on the following E2E post, and I want to make sure I am using the correct version of parameters 9 and 10: http://e2e.ti.com/support/dsp/c5000/f/109/p/119626/427368.aspx#427368


Thanks - AM

  • Hi AndMan,

     For the configuration you have mentioned: Clock Pol = 0  & FRMT = DSP format :  

     Receive data will be sampled on the falling edge and transmit data shifted on the rising edge of the bit clock.

     And according to data sheet ( parameters 9 and 10) :

      tsu(FSV-CLKH)  = Setup time, I2S_FS valid before I2S_CLK high (CLKPOL = 0) ,

      th(CLKH-FSV) =  Hold time, I2S_FS valid after I2S_CLK high (CLKPOL = 0) -  which looks correct.

     Below is the snapshot for the above mentioned timing details from datasheet:

    Hope the information helps.

    Regards

     Vasanth