I have a question about SPI AEL/AFL size. In document spru73h, the range is 1~64. BUT, in document spru73j the range is 1~256. Which one is correct? If the range is 1~256, does it mean the fifo size is 256 bytes?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The McSPI FIFO is 64 bytes. If you are referring to the MCSPI_XFERLEVEL register fields, these have been corrected from TRM Rev. I on. The latest revision is J. The fact that AEL/AFL field values can be up to 0xFF does not mean that the FIFO is 256 bytes. It's user responsibility to set the correct field values.