This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EEPROM programming error



Hi,

I am using EVM5515 and CCSv4. I can program NAND and NOR memory but some error occurs when i try to program SPI EEPROM or IIC EEPROM.

I am using programmer.out to download bin file to memory (cleaner.bin). I can do it fine for NAND and NOR but for EEPROM:

Choose the device...

0XX - CPLD setup only

1x - NAND Flash [CSx: 2,3,4,5]

2x - NOR Flash [CSx: 2,3,4,5]

3x - SPI EEPROM [x=1: EVM, x=2: USB Stick]

4 - IIC EEPROM

5 - MMC;  6 - SD

4

Operation to perform...

0 - CPLD setup for this device

1<file> - Program device with <file>

2<file> - Read device data to output <file>

1C:\Users\atornes\Desktop\cleaner.bin

IIC EEPROM...

Writing data to device...

Opening C:\Users\atornes\Desktop\cleaner.bin...

Input file opened

WRITE ERROR! at 0x0000

Wrote 0x0001  Read 0x0000

Any help?

Thank you