Other Parts Discussed in Thread: AM3356
I want to boot a AM3356 from a 1.8V eMMC, but I'm struggling with a certain phrase in the technical reference manual (SPRUH73I). Else where the MMC1 port is described as supporting both 1.8V and 3.3V.
26.1.7.5.4 Initialization and Detection
The ROM Code initializes the memory device or card connected on MMC interface using the standard
High-Voltage range (3.3 V).
Does this mean that it's not possible to boot from a 1.8V eMMC, and if so can someone explain the reason why?
The pins are powered from VDDSHV1 which in my case is 1.8V. How should the register settings in register SD_CAPA (VS18, VS30, VS33), and register SD_HCTL (SDVS) be understood/used?
Thomas