Hello,
I am using Advantech's DSPC-8681e card and trying to get some network throughput measurements and run other network tests. I have taken the PA emac example and modified it to get it working with one chip on the card.
If I connect the card to a router with other PCs connected, I can send packets from the card to other PCs on the router and receive packets from the other PCs as well. Looking at the lights on the ethernet port when the cable is plugged in, I can see that the green light is on indicating a GbE connection.
If I try to instead connect a Superlooper GbE loopback plug to the card, no ethernet lights come on at all. Is there any additional or different setup needed for a loopback connector? Is there a recommended loopback connector to use or are there any possible problems with the one I am using?
The one I am using is here: http://www.cablesandkits.com/superlooper-gigabit-loopback-tool-p-1682.html?CAWELAID=120126460000010226&gclid=CJng5PHxg74CFa_m7Aod4TQArg
Chris