Other Parts Discussed in Thread: TM4C129XNCZAD
Hi,
I tried to debug the tcpecho example project on DK-TM129X on TI-RTOS, but it gave me "
Invalid CIO command (0). Memory map prevented reading 0x2000E7D8" error when I tried to run it.
The project that I load was : tcpEcho_TivaTM4C129XNCZAD .
And based on the debugging that I have done, seems like it is due to the system_printf call...(after executing system_flush())
But, If I tried other project, for example gpio_interrupt project , everything worked fine. The system_printf run fine too !
Do I need to set something to make the udpecho project work ?
The same error happened on tcpecho project as well.
Thank you